Skip to main content
Visitor II
Sep 24, 2025 7:59 AM UTC
Question

STM32G474 On-the-Fly Flash Update: Handling ramfunc and CCMRAM Functions

Currently, on the STM32G474, I am able to perform on-the-fly flash operations and interrupt vector relocation using BF_MODE and VTOR.

However, I have encountered an issue: when a function is placed in RAM using the ramfunc attribute or located in CCMRAM, how can I still achieve on-the-fly operation?

This topic has been closed for replies.

1 reply

ST Technical Moderator
Sep 30, 2025 8:59 AM UTC

Hello @Leo_Yang_1985 ,

Yo may find recommendations in this application note AN4296 to optimize performance when using CCMRAM for code execution. Make sure that the code execution is not affected by cache behavior as described in the errata-sheet.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks