Skip to main content
Calypso 2021
Associate II
Nov 18, 2026 3:00 PM UTC
Question

STM32G474 HRTIM: fast EEV in RSTx2R works with DTEN=1 – supported?

Hello,

STM32G474, HRTIM Timer C, TC1/TC2 complementary with deadtime (DTEN=1).
TC2 reset source = EEV4 (COMP1, level, active low).

Result:
- EE4FAST = 0: no effect on TC2
- EE4FAST = 1: TC2 held low while EEV4 is active; TC1 unaffected; TC2 resumes normally on release

RM0440 p. 910 says RSTx2R is "not significant when DTEN bit is set", but CubeMX allows this setting, and the EExFAST description says the event is "acting asynchronously on outputs".

Is this a supported way to force output 2 inactive with deadtime enabled? And does the fast path act after the deadtime unit, so deadtime is always kept on release?

Thanks.

1 reply

mƎALLEm
ST Technical Moderator
Nov 20, 2026 4:33 PM UTC

Hello ​@Calypso 2021 ,

Your request has been raised internally over this internal ticket number:  CDM0067689 (not accessible by the community users).

I’ll get back to you as soon as I have any feedback.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.