STM32G474, HRTIM Blanking / Windowing documentation is contradictory
- 3 replies
- 1663 views
I need to detect if there is a comparator state change inside a PWM pulse. I want to look for this a little after the PWM rising edge and stop before the PWM falling edge.
The PWM is running in center aligned mode.
RM0440, Rev 4, STM32G4 Reference manual:
1) Page 884 last paragraph says: "Whenever the roll-over event is used for blanking or windowing, the ROM[1:0] programming applies for defining when it is generated"
2) Page 894 first bullet says: "In up/down mode (UDM bit set to 1), the counter reset event is defined as per the ROM[1:0] bit setting.
Section 27.5.49, page 1028 defines ROM[1:0]. It says for case
00: Event generate when the counter is equal to 0 or to HRTIM_PERxR value
01: ...
Let's say I program:
Period to 1000, PWM to 400 and compare 1 to 500. This means from 0 to 400 the PWM output is low, from 400 up to 1000 down to 400 the PWM output is high and then from 399 to 0 the PWM output is low. I want the blanking window to be open between 500 up to 1000 down to 500.
I then program EE1FLTR[3:0] in HRTIM_EEFxR1 (page 999) to:
0001: Blanking from counter reset/roll-over to compare 1
If program ROM[1:0] to 00. Will I get:
A) Blanking from 0 to 499 and the no blanking from 500 up to 1000 down to 500 and then blanking from 499 down to 0
or
B) Blanking from 0 to 499 and the no blanking from 500 up to 1000. Then blanking from 999 down to 500 and then no blanking from 499 down to 0?
It must be A otherwise, this is a bug and a terrible implementation.
Can I please get clarification of the behavior of blanking (and windowing) in up/down mode for the different ROM[1:0] and EE1FLTR[3:0] settings?
I've attached a PDF file with the relevant portions from the manual.