STM32G474: CAN-Bus clock and timing setup
- November 13, 2021
- 4 replies
- 10544 views
Hello,
regarding the STM32G474 I have some questions regarding the CAN Controller:
1) The CAN-Controller has an input called “fdcan_clk�?, is this connected to APB1-peripheral-clocks?
2) How does the CCU work to generate the fdcan_tq_ck, how should it be set up?
I found very little information about it, what would be a recommendation for a 500kBit/s CAN2.0B setup.
I assume the calibration-feature is most likely be used in the CAN-FD Mode, I may use that in the future. If someone has more details how set up, I would really be interested as well.
Many thanks for helping in advance.
Best Regards, Seppel
P.S. I also found different diagrams( RM0440 Rev 6 vs. AN5348 - Rev 1), not sure why that is the case. I also did not find where the registers are described in detail.