Skip to main content
Associate
May 23, 2025 2:15 AM UTC
Question

STM32G473VET3 SPI master NSS

Hi ST teams,

I use STM32G473VET3 on my design. On the datasheet, SPI4 had 3 NSS pins hardware: PE3, PE4 and PE11.

If I use other GPIO excluding for the NSS pin function, there are any potential issue?
Ex: SPI bus can not work at maximum speed.

On my design, I use SPI4 is master and PF2, PF9, PE3, PE4, PE5 for slave chip select function.

Thanks.

 

This topic has been closed for replies.

3 replies

TDK
May 23, 2025 2:22 AM UTC

If you're controlling the CS/NSS pins manually (GPIO output and toggle), there are no downsides to choosing a different pin. It won't affect max clock rate.

If you have multiple slaves, you have no choice but to control CS/NSS manually.

"If you feel a post has answered your question, please click ""Accept as Solution""."
HoangDuAuthor
Associate
May 23, 2025 2:33 AM UTC

Thank you for reply.

So i understand that there are no issue/limited when control CS/NSS manually instead use "automatic" CS/NSS control?

TDK
May 27, 2025 12:37 AM UTC

Yes

"If you feel a post has answered your question, please click ""Accept as Solution""."