Skip to main content
wb0gaz
Associate III
January 29, 2024
Solved

STM32G473/4 FMC/FSMC feature, pin called FMC_NL and FMC_NADV in datasheet DS12712 rev 5

I'm working on migrating a design from STM32F405 series to STM32G473 series, both LQFP100 package, both use FSMC for access to external SRAM (in multiplexed mode; I have separate address latches clocked from FMC_NADV capturing A0..A15 from D0..D15.)

When verifying pin-by-pin alternate function definitions, I encountered FMC_NL (assigned through PB7) where I expected to find FMC_NADV (assigned through PB7.)

On further checking, I see that datasheet for G473 (DS12712 rev 5 is the version I downloaded and am referencing) cites FMC_NL only in the pin/alternate function definitions, and FMC_NADV in the timing diagrams.

The reference manual (RM0440) doesn't appear to site either pin name.

Is reference FMC_NL in the pin alternate function definitions to be taken as a typo which should read FMC_NADV?

Thank you

 

This topic has been closed for replies.
FBLBest answer
ST Technical Moderator
January 30, 2024

Hello @wb0gaz 

It is already mentioned in the reference manual figure 52. FMC_NL (or NADV) 

FBelaid_0-1706604392318.png

I agree, it should have been explicitly detailed in the datasheet.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL

1 reply

FBLBest answer
ST Technical Moderator
January 30, 2024

Hello @wb0gaz 

It is already mentioned in the reference manual figure 52. FMC_NL (or NADV) 

FBelaid_0-1706604392318.png

I agree, it should have been explicitly detailed in the datasheet.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL