Skip to main content
Associate
November 17, 2023
Solved

STM32G431KB Nucleo 32 - USART1 RX help

I'm trying to use USART1 for Async however I cannot send data to the board. I'm using an FTDI USB-UART converter cable to test, the Nucleo is sending correct data my PC data no problem.

I can prove my code and terminal program on the PC works 2 way with the USART2 and VCP via STLINK.

When code is set to use USART1. USART1_Rx has nothing coming in.

I saw a reference in the UM for USART1:

"Only one USART is available and shared between ARDUINO® Nano and VCP. The selection is done by remapping (no need to change the hardware configuration)."

I think there might be something I don't understand about this. I have done the "remapping" with cube MX to assign the default UART1 pins PA9&10.

Any guidance is welcome on how to get Rx working.

This topic has been closed for replies.
LiamRDSBest answer
Associate
November 20, 2023

It turned out that I was getting ORE after the first time my device send data to the STM32, it did work briefly however thereafter the Rx of course would not work.

I eventually just turned that off overrun CubeMX and it seems solid so far for this purpose.

Thanks for the help everyone.

4 replies

STTwo-32
ST Technical Moderator
November 17, 2023

Hello @LiamRDS

I suggest you compare your UART configurations to the UART configuration in one of the provided examples. That will help you locating the issue. 

PS: It will be better if you share your code.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Pavel A.
November 17, 2023

Check the flow control pins on the FTDI side (CTS/DSR). Try other, simpler USB-UART converter (Prolific..).

Karl Yamashita
Principal
November 17, 2023

I have a Nucleo-G431KB and USART1 works on PA9 and PA10. Maybe put the FTDI in loopback to make sure it works? The only other thing to check if you have NVIC enabled?

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
LiamRDSAuthorBest answer
Associate
November 20, 2023

It turned out that I was getting ORE after the first time my device send data to the STM32, it did work briefly however thereafter the Rx of course would not work.

I eventually just turned that off overrun CubeMX and it seems solid so far for this purpose.

Thanks for the help everyone.