Skip to main content
July 25, 2024
Solved

STM32G431 Comparator output to Timer

Hello.

STM32G431CBT6

Is it possible to route the output from the comparator to the input of the Timer input? The reference manual says that this is possible, but there is no description. And in the comparator register there are no options for choosing where to send the output.
Previously, I used stm32f072, and in the comparator settings there is an "OUTSEL"  bit field where you can select where the output will be connected.

I need to measure the signal period (timer in "input capture" mode). 

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
July 25, 2024

In 'G4, the interconnection from comparators to timers is extensive.

For interconnection into the individual channels, see description of TIMx_TISEL register(s) and the links to the input matrix tables from there.

JW

2 replies

waclawek.jan
waclawek.janBest answer
Super User
July 25, 2024

In 'G4, the interconnection from comparators to timers is extensive.

For interconnection into the individual channels, see description of TIMx_TISEL register(s) and the links to the input matrix tables from there.

JW

MM..1
Super User
October 20, 2024

I extend question here. When i set comparator out to timer capture and plan measure time on failing edges , result is problem. Tim generate event too on signal from comparator out rising. On scope zoom i see some very short pulses at the comparator level changes. Hysteresis is set to medium, but problem persist. 

Result is comparators unusable in MCU offload and require some IRQ control for this short pulse ignore.

Tested with internal reference or DAC out = same results.