Skip to main content
Associate
Jan 8, 2026 1:03 PM UTC
Solved

STM32G4: Wrong description of HRTIM_ADCxR registers in RM0440 Rev 9

If I am correct, the descriptions of
 - HRTIM_ADC2R
   -  Bit 22
 - HRTIM_ADC3R
   - Bit 19
   - Bit 13
 - HRTIM_ADC3R
   - Bit 22
   - Bit 13
   - Bit 10
   - Bit 5
   - Bit 4
   - Bit 0
are not correct in the RM.

They all describe trigger event generation but the trigger output in all these seem wrong:
E.g.: HRTIM_ADC2R, Bit 22,
Original Text: "This bit enables the generation of an ADC trigger upon timer C reset and roll-over event, on ADC trigger 1 output."
It should be: "This bit enables the generation of an ADC trigger upon timer C reset and roll-over event, on ADC trigger 2 output."

Also, I want to ask, if this forum is the right place to give feedback on documentation issues?

Best Simon

Imen.DBest answer
ST Technical Moderator
Jan 8, 2026 6:37 PM UTC

Hello @simountain and welcome to the Community,

Thank you for bringing this issue to our attention.

An internal ticket number 224817 is submitted in order to fix this. 

 

Also, I want to ask, if this forum is the right place to give feedback on documentation issues?


Yes, this is the right place to share this kind of feedback and report issues. Please feel free to share them with us here.

Thank you for your contributions.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

1 reply

Imen.DBest answer
ST Technical Moderator
Jan 8, 2026 6:37 PM UTC

Hello @simountain and welcome to the Community,

Thank you for bringing this issue to our attention.

An internal ticket number 224817 is submitted in order to fix this. 

 

Also, I want to ask, if this forum is the right place to give feedback on documentation issues?


Yes, this is the right place to share this kind of feedback and report issues. Please feel free to share them with us here.

Thank you for your contributions.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks