Skip to main content
Terry Greeniaus
Senior
April 14, 2020
Question

STM32G4 PLL documentation errors

  • April 14, 2020
  • 1 reply
  • 647 views

Hi,

The documentation between the STM32G4 RM0440 Rev 3 and between the individual MCU specifications is inconsistent when it comes to the PLL limits. In the documentation for RCC_PLLCFGR we have the following two statements:

PLLN: "The software has to set correctly these bits to assure that the VCO output frequency is between 64 and 344 MHz."

PLLM: "The software has to set these bits correctly to ensure that the VCO input frequency ranges from 2.66 MHz to 8 MHz."

However, in DS12288 Rev 2 (data sheet for STM32G474xB xC and xE), under "5.3.9 PLL Characteristics", we have the following limits:

fVCO_OUT: 96 MHz to 344 MHz (Range 1) or 96 MHz to 128 MHz (Range 2)

fPLL_IN: 2.66 MHz to 16 MHz

Could we get clarification on what the correct limits are?

Thanks!

This topic has been closed for replies.

1 reply

ST Technical Moderator
April 14, 2020

Hello @Terry Greeniaus​ ,

Thank you for highlighting this.

The correct values of "PLL Characteristics" are in the datasheets.

We will modify RM0440 and remove wrong statements (there should be no numeric values – just reference to datasheet).

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks