Skip to main content
Associate III
September 15, 2025
Solved

STM32G0x ADC CFGR1 clears Resolution bits on EXTSEL bit modification

Hi, 

 

When I clear the EXTSEL bits in the ADC1 CFGR1 register, my resolution bits also get cleared ?. My ADC randomly changes resolution. Below is screenshots of the code. 

danielbathtub_0-1757929118143.png

 

Why does this happen ?, I can disable the ADC to write the RES bits to what they were. Don't really want to do that unless I have to. 

This topic has been closed for replies.
KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
September 15, 2025

Hello @danielbathtub ;

 

When you writing any bits in the ADC_CFGR1 register of STM32G0x while the ADC is enabled (ADEN bit set), the RES[1:0] (resolution) bits are reset. This behavior is documented in STM32G0 errata sheets like as in STM32G050 errata sheet.

KDJEM1_0-1757942377138.png

 

 

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.

2 replies

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
September 15, 2025

Hello @danielbathtub ;

 

When you writing any bits in the ADC_CFGR1 register of STM32G0x while the ADC is enabled (ADEN bit set), the RES[1:0] (resolution) bits are reset. This behavior is documented in STM32G0 errata sheets like as in STM32G050 errata sheet.

KDJEM1_0-1757942377138.png

 

 

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
MKANO.2
ST Employee
September 15, 2025

 

Hi danielbathtub,                                                                                                                                                           The issue is already documented in Errata sheet ES0545 - Rev 3 that when modifying the ADC_CFGR1 register while ADEN bit is set  will resets RES[1:0] bit . A workaround is proposed for that.                                                          Mariem