Skip to main content
Associate
Jun 9, 2026 10:56 AM UTC
Solved

STM32G0B1VET6 USB boot

Hi,

I am using an STM32G0B1VET6. All power rails in my design, including VDDIO2/VDDUSB, are supplied from 3.0 V (2.95 min).

I would like to use the USB interface and the built-in USB DFU bootloader for firmware updates.

AN2606 states that VDDUSB must be connected to 3.3 V. However, AN4879 appears to specify a USB supply operating range down to 2.7 V, with 3.0 V as the minimum recommended operating voltage in some cases. Based on that, I would expect USB to operate correctly with VDDUSB supplied from 3.0 V.

Could you please confirm whether USB DFU is supported on the STM32G0B1 when VDDUSB/VDDIO2 is powered from 3.0 V rather than 3.3 V?

The board will be powered from its own 3.0 V supply. For the USB programming connection, I am planning to bring out only three wires:

  • USB D+
  • USB D−
  • GND

The USB 5 V VBUS line will not be used to power the board.

Are these three connections sufficient for entering the system bootloader and performing a firmware update through USB DFU, or is the USB VBUS line or a separate VBUS-detection signal also required?

Thank you.

TDK
TDKBest answer
Jun 9, 2026 7:25 PM UTC

The data sheet has the correct information. AN2606 is just some copy/paste note.

3.0 V is sufficient for USB operation. VBUS is not used. Only D+/D-/GND need connected for correct functionality.

Technically, if the device is self-powered, you need to monitor VBUS before energizing the data lines per the USB standard, but this is not required in practice.

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

MM..1
Super User
Jun 9, 2026 4:13 PM UTC

Why you first not test with 3V3 ??? Condition for boot is in AN2606
and VDDUSBIO writed in AN 3V3 mean require power, value isnt strict.

TDK
TDKBest answer
Jun 9, 2026 7:25 PM UTC

The data sheet has the correct information. AN2606 is just some copy/paste note.

3.0 V is sufficient for USB operation. VBUS is not used. Only D+/D-/GND need connected for correct functionality.

Technically, if the device is self-powered, you need to monitor VBUS before energizing the data lines per the USB standard, but this is not required in practice.

"If you feel a post has answered your question, please click ""Accept as Solution""."