Skip to main content
Visitor II
Jul 24, 2026 9:31 AM UTC
Solved

STM32G0B1RE - Need Independent PWM Frequencies on TIM1 Channels (PA8, PA9, PC11)

I'm working on an STM32G0B1RE and have a question regarding PWM generation and timer limitations.

 

Current Hardware Configuration

The hardware design is already fixed, so changing pins is difficult. Current PWM signals are routed as follows:
    PA8 -> TIM1_CH1
    PA9 -> TIM1_CH2
    PC11 -> TIM1_CH4
    PC9 -> TIM3_CH4
From CubeMX I confirmed that:
    PA8 -> TIM1_CH1 only
    PA9 -> TIM1_CH2, TIM15_BKIN
    PC11 -> TIM1_CH4 only
    PC9 -> TIM3_CH4, TIM1_CH2
My software currently uses TIM1_CH1, TIM1_CH2, and TIM1_CH4 simultaneously.

 

What I Observed
I have a PWM abstraction layer that allows setting frequency per logical PWM device. However, after reviewing the implementation and STM32 timer architecture, I realized that changing the frequency of one TIM1 channel modifies the timer ARR value, which affects all channels on TIM1. 
    DeviceA -> TIM1_CH1
    DeviceB -> TIM1_CH2
    DeviceC -> TIM1_CH4
If I execute:
    setFrequency(DeviceA, 1000);
and later:
    setFrequency(DeviceB, 5000);
the second call changes the TIM1 ARR register, causing all TIM1 channels to run at 5 kHz. This seems expected since TIM1 channels share:
    PSC
    ARR
    Counter
and only have independent CCR registers.

 

Requirement
Ideally I would like something like:
    PA8 (TIM1_CH1) -> 1 kHz
    PA9 (TIM1_CH2) -> 2 kHz
    PC11 (TIM1_CH4) -> 5 kHz
running simultaneously.

 

My Questions
1.    Is there any STM32 timer configuration or mode that allows different PWM frequencies on TIM1_CH1, TIM1_CH2, and TIM1_CH4 simultaneously while using the same TIM1 peripheral?
2.    My understanding is that with the current routing I effectively have only:
    TIM1 -> PA8, PA9, PC11
    TIM3 -> PC9
which means only two independent hardware PWM frequency domains are available?

Can someone confirm whether this understanding is correct and suggest the best approach?

Thanks in advance.
 

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Sep 4, 2026 8:51 AM UTC

Hello ​@ramesh6859 and sorry for the late reply,

1.    Is there any STM32 timer configuration or mode that allows different PWM frequencies on TIM1_CH1, TIM1_CH2, and TIM1_CH4 simultaneously while using the same TIM1 peripheral?

No. As you’ve already understood, the different same timer channels share the same registers: PSC, ARR and the Counter. So you can't generate several different PWM frequencies with the same timer.

2.    My understanding is that with the current routing I effectively have only:
    TIM1 -> PA8, PA9, PC11
    TIM3 -> PC9

Yes, due to your hardware constraint.

Hope that answers your question.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Sep 4, 2026 8:51 AM UTC

Hello ​@ramesh6859 and sorry for the late reply,

1.    Is there any STM32 timer configuration or mode that allows different PWM frequencies on TIM1_CH1, TIM1_CH2, and TIM1_CH4 simultaneously while using the same TIM1 peripheral?

No. As you’ve already understood, the different same timer channels share the same registers: PSC, ARR and the Counter. So you can't generate several different PWM frequencies with the same timer.

2.    My understanding is that with the current routing I effectively have only:
    TIM1 -> PA8, PA9, PC11
    TIM3 -> PC9

Yes, due to your hardware constraint.

Hope that answers your question.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.