Skip to main content
Associate II
Mar 25, 2026 7:38 AM UTC
Solved

STM32G0B1KCT6 how to use dual bank as single bank to use full 256KB.

I am using STM32G0B1KCT6 MCU, i would like to use the full flash of 256KB starting from 0x8000000 to 0x803FFFF. but am unable to flash in bank 2 (ranging from 0x8020000 to 0x803FFFF).
if i reduce the flash size to Bank1 only, then am able to flash and run the code.
I am aware its default dual bank MCU. PFA code snippet for changing it to single bank.
Also tried changing it single bank using the stcubeprogrammer but still fails to flash the MCU.

 
 
 
void ConfigureFlashToSingleBank(void)
{
 FLASH_OBProgramInitTypeDef OBInit;

 HAL_FLASHEx_OBGetConfig(&OBInit);

 /* Check if Dual Bank mode is enabled */
 if (OBInit.USERConfig & FLASH_OPTR_DUAL_BANK)
 {
 HAL_FLASH_Unlock();
 HAL_FLASH_OB_Unlock();

 OBInit.OptionType = OPTIONBYTE_USER;

 /* Disable Dual Bank (enable linear 256KB flash) */
 OBInit.USERConfig &= ~FLASH_OPTR_DUAL_BANK;

 if (HAL_FLASHEx_OBProgram(&OBInit) == HAL_OK)
 {
 HAL_FLASH_OB_Launch(); // triggers reset
 }

 HAL_FLASH_OB_Lock();
 HAL_FLASH_Lock();
 }
}

 the .icf file for the same is 

/*###ICF### Section handled by ICF editor, don't touch! ****/
/*-Editor annotation file-*/
/* IcfEditorFile="$TOOLKIT_DIR$\config\ide\IcfEditor\cortex_v1_0.xml" */
/*-Specials-*/
define symbol __ICFEDIT_intvec_start__ = 0x08000000;
/*-Memory Regions-*/
define symbol __ICFEDIT_region_ROM_start__ = 0x08000000;
define symbol __ICFEDIT_region_ROM_end__ = 0x0803FFFF;
define symbol __ICFEDIT_region_RAM_start__ = 0x20000000;
define symbol __ICFEDIT_region_RAM_end__ = 0x20023FFB;

/*-Sizes-*/
define symbol __ICFEDIT_size_cstack__ = 0x400;
define symbol __ICFEDIT_size_heap__ = 0x200;
/**** End of ICF editor section. ###ICF###*/

define memory mem with size = 4G;
define region ROM_region = mem:[from __ICFEDIT_region_ROM_start__ to __ICFEDIT_region_ROM_end__];
define region RAM_region = mem:[from __ICFEDIT_region_RAM_start__ to __ICFEDIT_region_RAM_end__];

define block CSTACK with alignment = 8, size = __ICFEDIT_size_cstack__ { };
define block HEAP with alignment = 8, size = __ICFEDIT_size_heap__ { };

initialize by copy { readwrite };
do not initialize { section .noinit };

place at address mem:__ICFEDIT_intvec_start__ { readonly section .intvec };

place in ROM_region { readonly };
place in RAM_region { readwrite,
 block CSTACK, block HEAP };

export symbol __ICFEDIT_region_RAM_start__;
export symbol __ICFEDIT_region_RAM_end__;

Also the flash region defined for dfu use is used as @Internal Flash /0x08000000/128*002Kg where it fails ...
but works when reduced to single bank with flash region defined as @Internal Flash /0x08000000/64*002Kg 

 

Attached image error appears when tried flashing through the IAR IDE. 
How do i resolve this to use full flash as single bank without bank separation.
Please guide through to work as per the requirement

 

SnehaBest answer
Associate II
Apr 16, 2026 9:35 AM UTC

The IAR IDE flasher used by the for flashing the MCU via debugger used the below attached files and spec that defines the banks separately and does not allow write over bank2. 

Sneha_0-1776331759860.png

These files are now modified with full memory usage for the given MCU., which now allows writing into BANK2.

Sneha_1-1776332030780.pngSneha_2-1776332070912.pngSneha_3-1776332109911.png

Regards,

Sneha

6 replies

mƎALLEm
ST Technical Moderator
Mar 25, 2026 9:41 AM UTC

Hello,

Check if you have enabled any security feature starting from BANK2 address: for example the FLASH write protection (WRP).

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
SnehaAuthor
Associate II
Mar 25, 2026 9:59 AM UTC
 
 

Hi.,
Write protection on the MCU is disabled.

Thanks and regards,

Sneha

mƎALLEm
ST Technical Moderator
Mar 25, 2026 10:02 AM UTC

Are you able to erase all the Flash and to write to the second bank using CubeProgrammer?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
SnehaAuthorBest answer
Associate II
Apr 16, 2026 9:35 AM UTC

The IAR IDE flasher used by the for flashing the MCU via debugger used the below attached files and spec that defines the banks separately and does not allow write over bank2. 

Sneha_0-1776331759860.png

These files are now modified with full memory usage for the given MCU., which now allows writing into BANK2.

Sneha_1-1776332030780.pngSneha_2-1776332070912.pngSneha_3-1776332109911.png

Regards,

Sneha