Skip to main content
Visitor II
Apr 21, 2026 1:54 PM UTC
Question

STM32G0B1CBT3N vs STM32G0B1CBT6N

Hello Peter , 

Need your expert reply 

As we see , the confusion on N AND no N HAS MADE many of us wonder , if these can be used as  interchangeable parts . Since Data Sheet does not explain , much on them ,But a search explains a compact Solution in Io's for a design flexibility . 

As both have same Packages and Pin  Count . 

We are in need for DESIGN - STM32G0B1CBT3N , but seems to be difficult  to procure  . Is this Manufactured or is it rare . We only See STM32G0B1CBT6N 

 

Regards

Nitin

1 reply

Peter BENSCH
ST Technical Moderator
Apr 21, 2026 2:25 PM UTC

Welcome @Tintin33, to the community!

By looking at the product website for the STM32G0B1CB, it can be seen that there is currently no STM32G0B1CBT3N (-40...+125°C). At present, therefore, you only have the option of using the STM32G0B1CBT6N (-40...+85°C).

If you absolutely need the wider temperature range, you will need to clarify availability with your local distributor, which will in any case require a minimum order quantity to release this variant - assuming that this is even possible at high temperatures because of the added functionality (VDDIO2 and UCPD).

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.