Skip to main content
ŁJura.1
Associate II
July 11, 2024
Solved

STM32G0B1, CANFD issues

Hi guys!

I have a custom board with 2x CAN FD transcievers (TCAN1057) and STM32G0B1 MCU. Everything works fine until i try to use hardware filters build into STM32. Whatever i do, filters don't pass any frame to RxFifo0/RxFifo1. The only way to recieve anything is to configure global filter with FDCAN_ACCEPT_IN_RX_FIFO0 option. With code pasted below, HAL_FDCAN_IRQHandler  is never called. Temporary i used workaround with global filter and hardcoded frame ID check, but i would like to solve the issue anyway. Can someone give me some advice?

 

The code:

https://pastebin.com/p7GVU1F7

 

BR.

Łukasz

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
September 20, 2024

Hello @ŁJura.1 ,

Any status on your progress in this case?

Edit:

Looking again at your code, the filters number in your config are set to 0.

 hfdcan1.Init.StdFiltersNbr = 0;
 hfdcan1.Init.ExtFiltersNbr = 0;

 You need to set at least one filter for each CAN frame type (Standard and Extended).

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

6 replies

ŁJura.1
ŁJura.1Author
Associate II
July 12, 2024

Nobody?

nouirakh
ST Employee
July 16, 2024

Hello @ŁJura.1 

The link you shared with us is unreachable. Could you please share your code here by using the option "Insert/Edit code simple".
Otherwise, Can you ensure that the filter configuration is correctly set up. Here is an example of how to configure a filter:

FDCAN_FilterTypeDef sFilterConfig;

sFilterConfig.IdType = FDCAN_STANDARD_ID; // or FDCAN_EXTENDED_ID
sFilterConfig.FilterIndex = 0;
sFilterConfig.FilterType = FDCAN_FILTER_MASK;
sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0; // or FDCAN_FILTER_TO_RXFIFO1
sFilterConfig.FilterID1 = 0x123; // Example ID
sFilterConfig.FilterID2 = 0x7FF; // Example Mask

if (HAL_FDCAN_ConfigFilter(&hfdcan, &sFilterConfig) != HAL_OK)
{
 // Filter configuration Error
 Error_Handler();
}

Also, you need to check Interrupt Configuration: 

HAL_NVIC_SetPriority(FDCAN1_IT0_IRQn, 0, 1);
HAL_NVIC_EnableIRQ(FDCAN1_IT0_IRQn);

Finaly, ensure that the FDCAN peripheral is correctly initialized before configuring filters and enabling interrupts:

if (HAL_FDCAN_Init(&hfdcan) != HAL_OK)
{
 // Initialization Error
 Error_Handler();
}

 

ŁJura.1
ŁJura.1Author
Associate II
July 17, 2024
 // 500kbps
 hfdcan1.Instance = FDCAN1;
 hfdcan1.Init.ClockDivider = FDCAN_CLOCK_DIV1;
 hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
 hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
 hfdcan1.Init.AutoRetransmission = ENABLE;
 hfdcan1.Init.TransmitPause = DISABLE;
 hfdcan1.Init.ProtocolException = DISABLE;
 hfdcan1.Init.NominalPrescaler = 16;
 hfdcan1.Init.NominalSyncJumpWidth = 1;
 hfdcan1.Init.NominalTimeSeg1 = 3;
 hfdcan1.Init.NominalTimeSeg2 = 4;
 hfdcan1.Init.DataPrescaler = 1;
 hfdcan1.Init.DataSyncJumpWidth = 1;
 hfdcan1.Init.DataTimeSeg1 = 1;
 hfdcan1.Init.DataTimeSeg2 = 1;
 hfdcan1.Init.StdFiltersNbr = 0;
 hfdcan1.Init.ExtFiltersNbr = 0;
 hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
 if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)
 {
 Error_Handler();
 }
 
 // 667kbps
 hfdcan2.Instance = FDCAN2;
 hfdcan2.Init.ClockDivider = FDCAN_CLOCK_DIV1;
 hfdcan2.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
 hfdcan2.Init.Mode = FDCAN_MODE_NORMAL;
 hfdcan2.Init.AutoRetransmission = ENABLE;
 hfdcan2.Init.TransmitPause = DISABLE;
 hfdcan2.Init.ProtocolException = DISABLE;
 hfdcan2.Init.NominalPrescaler = 8;
 hfdcan2.Init.NominalSyncJumpWidth = 1;
 hfdcan2.Init.NominalTimeSeg1 = 5;
 hfdcan2.Init.NominalTimeSeg2 = 6;
 hfdcan2.Init.DataPrescaler = 1;
 hfdcan2.Init.DataSyncJumpWidth = 1;
 hfdcan2.Init.DataTimeSeg1 = 1;
 hfdcan2.Init.DataTimeSeg2 = 1;
 hfdcan2.Init.StdFiltersNbr = 0;
 hfdcan2.Init.ExtFiltersNbr = 0;
 hfdcan2.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
 if (HAL_FDCAN_Init(&hfdcan2) != HAL_OK)
 {
 Error_Handler();
 }
 
 // pass anything from any can instance to fifo0
 // it also doeant work if i use values like 0x18FA0000 / 0x1FFF0000
 FDCAN_FilterTypeDef sFilterConfig;
 sFilterConfig.IdType = FDCAN_EXTENDED_ID;
 sFilterConfig.FilterIndex = 1;
 sFilterConfig.FilterType = FDCAN_FILTER_MASK;
 sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
 sFilterConfig.FilterID1 = 0x0000000;
 sFilterConfig.FilterID2 = 0x0000000;
 
 
 
 if (HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig) != HAL_OK)
 {
 /* Filter configuration Error */
 Error_Handler();
 }
 if (HAL_FDCAN_ConfigFilter(&hfdcan2, &sFilterConfig) != HAL_OK)
 {
 /* Filter configuration Error */
 Error_Handler();
 }
 
 // this works
// HAL_FDCAN_ConfigGlobalFilter(&hfdcan1, FDCAN_ACCEPT_IN_RX_FIFO0, FDCAN_ACCEPT_IN_RX_FIFO0, FDCAN_FILTER_REMOTE, FDCAN_FILTER_REMOTE);
// HAL_FDCAN_ConfigGlobalFilter(&hfdcan2, FDCAN_ACCEPT_IN_RX_FIFO0, FDCAN_ACCEPT_IN_RX_FIFO0, FDCAN_FILTER_REMOTE, FDCAN_FILTER_REMOTE);
 
 
 // this doesn't work
 HAL_FDCAN_ConfigGlobalFilter(&hfdcan1, FDCAN_REJECT, FDCAN_REJECT, FDCAN_FILTER_REMOTE, FDCAN_FILTER_REMOTE);
 HAL_FDCAN_ConfigGlobalFilter(&hfdcan2, FDCAN_REJECT, FDCAN_REJECT, FDCAN_FILTER_REMOTE, FDCAN_FILTER_REMOTE);
 
 // STart FDCAN1
 if(HAL_FDCAN_Start(&hfdcan1)!= HAL_OK)
 {
 Error_Handler();
 }
 
 // STart FDCAN2
 if(HAL_FDCAN_Start(&hfdcan2)!= HAL_OK)
 {
 Error_Handler();
 }
 
 // Activate the notification for new data in FIFO0 for FDCAN1
 if (HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0) != HAL_OK)
 {
 /* Notification Error */
 Error_Handler();
 }
 
 
 // Activate the notification for new data in FIFO0 for FDCAN2
 if (HAL_FDCAN_ActivateNotification(&hfdcan2, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0) != HAL_OK)
 {
 /* Notification Error */
 Error_Handler();
 }

 

Here is the same code, hope now it's visible.
 

mƎALLEm
ST Technical Moderator
July 16, 2024

Hello,

Before using Normal mode, start by using Loopback mode to validate your filters config. If you face an issue share your project.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
ŁJura.1
ŁJura.1Author
Associate II
July 17, 2024

Ok, i'll try and report.

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
September 20, 2024

Hello @ŁJura.1 ,

Any status on your progress in this case?

Edit:

Looking again at your code, the filters number in your config are set to 0.

 hfdcan1.Init.StdFiltersNbr = 0;
 hfdcan1.Init.ExtFiltersNbr = 0;

 You need to set at least one filter for each CAN frame type (Standard and Extended).

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.