STM32G070RB: Inconsistent FLASH_ACR EMPTY flag after full erase (REV_ID 0x2000 vs 0x2001)
- 1 reply
- 270 views
Hello everyone,
I'm observing inconsistent FLASH ACR EMPTY flag behavior on two STM32G070RB chips (DEV_ID 0x6460) after a full chip erase by using STM32CubeProgrammer]
Observed behavior:
STM32G070RB (REV_ID 0x2000): After full erase, FLASH_ACR EMPTY flag correctly sets to '1' (chip boots into system memory). This is the expected behavior.
STM32G070RB (REV_ID 0x2001): After full erase, FLASH_ACR EMPTY flag remains '0'. The chip attempts to boot from main Flash (0x08000000) despite being empty, leading to unexpected behavior.
Questions:
Is there a documented difference in the Flash empty check mechanism or FLASH_ACR EMPTY flag behavior between STM32G070RB REV_ID 0x2000 and REV_ID 0x2001?
Are specific option byte settings or erase sequences required for REV_ID 0x2001 to correctly assert the EMPTY flag after a full erase? (I have tried power cycling.)
Thanks,
Tomislav