Skip to main content
Associate III
Dec 29, 2025 12:19 PM UTC
Question

STM32G070 software reset issue

I was doing reset through SPI command and expected results are not happening.

 

this is the line i was expecting to reset the MCU

SCB->AIRCR = (NVIC_AIRCR_VECTKEY | (SCB->AIRCR & (0x700)) | (1 << NVIC_SYSRESETREQ));


where

#define NVIC_AIRCR_VECTKEY (0x05FA << 16)

#define NVIC_SYSRESETREQ 2

also my watchdog is running and expected to reset the system.
code snippet

 
FLASH_Unlock();
FLASH_ErasePage(0x08013000);
FLASH_ProgramWord(0x08013000, (uint64_t)0x0000000000000000ULL);
FLASH_Lock();

FLASH_Unlock();
FLASH_ErasePage(0x08013008);
FLASH_Lock();

SCB->AIRCR = (NVIC_AIRCR_VECTKEY | (SCB->AIRCR & (0x700)) | (1 << NVIC_SYSRESETREQ));
__DSB();

while (1);

 


Edited to apply proper source code formatting - please see How to insert source code for future reference.

12 replies

Andrew Neil
Super User
Dec 29, 2025 12:33 PM UTC

Please give some more details - see: How to write your question to maximize your chances to find a solution

 


@aravindpv wrote:

I was doing reset through SPI command and expected results are not happening..


So what, exactly, were you expecting to happen ?

What, exactly, is actually happening ?

What investigation/testing/debugging have you done to find the issue?

 


@aravindpv wrote:

this is the line i was expecting to reset the MCU.


Is that line ever executed?

Does it work without all the Flash stuff?

Without the SPI?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
aravindpvAuthor
Associate III
Dec 29, 2025 12:40 PM UTC

i was running a bootloader + main app setup on mcu where i expecting a particular command over SPI to capture one of my else condition and which is properly triggering. And on that condition i have added a reset line like mentioned above which is not happening or code executing but stuck at somewhere that kind of result I am getting. Actually my plan was to reset the mcu and set to start from 0x08000000 were my bootloader lies.

Andrew Neil
Super User
Dec 29, 2025 12:48 PM UTC

You didn't answer whether your reset line is ever getting executed?

 


@aravindpv wrote:

 i have added a reset line like mentioned above .


What do you mean, "like" ?

 

Why is that line doing a read-modify-write on SCB->AIRCR ?

Shouldn't it be just a write?

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
ST Technical Moderator
Dec 29, 2025 12:46 PM UTC

Hello,

Why complicate things to yourself? and why simply you don't use HAL_NVIC_SystemReset() to reset your MCU? You're already using HAL with the flash based on your shared code!

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
TDK
Dec 29, 2025 1:37 PM UTC

If HAL_NVIC_SystemReset doesn't reset the chip perhaps you have NRST tied high. Can't think of any other reason for it not working.

> But after reset, the RPi no longer sees the slave at 0x30

So it is resetting just not doing what you expect after reset?

"If you feel a post has answered your question, please click ""Accept as Solution""."
TDK
Dec 30, 2025 3:34 PM UTC

This looks like AI generated code with the comments. Maybe stick to the working HAL implementations to modify flash.

"If you feel a post has answered your question, please click ""Accept as Solution""."