Skip to main content
Associate
Jun 3, 2025 12:20 PM UTC
Solved

STM32G030K6T6 Timer 16 seems to use SYSCLK instead of PCLK

Hi all.

I have a small problem understanding the timer 16 of the STM32G030K6T6 microcontroller. According to the data sheet, it should use the TIMPCLK clock, which corresponds to the PCLK clock.
My system clock is supplied by the HSI (SYSCLK = 16 MHz). I have set my AHB prescaler to 4 and the APB prescaler to 1, so HCLK = PCLK = 4 MHz. Since my APB prescaler is equal to 1, the timer clock should be TIMPCLK = PCLK = 4 MHz.
I then implemented a delay function with timer 16. So that the counter runs up in 1 us steps, I have to set the prescaler of the timer to 15 instead of 3. This means that the timer 16 still has a 16 MHz signal as an input signal.
Now my question is: Have I misunderstood something here, is the data sheet wrong or is my code not correct? I have attached the quotes from the data sheet and my code. I hope you can help me.

 

 

Datasheet RM0454 Rev 5:

"Timer clock
The timer clock TIMPCLK is derived from PCLK (used for APB) as follows:
1. If the APB prescaler is set to 1, TIMPCLK frequency is equal to PCLK frequency.
2. Otherwise, the TIMPCLK frequency is set to twice the PCLK frequency."

 

"The peripherals are clocked with the clocks from the bus they are attached to (HCLK for
AHB, PCLK for APB) except:
• TIMx, with these clock sources to select from:
– TIMPCLK (selectable for all timers) running at PCLK frequency if the APB
prescaler division factor is set to 1, or at twice the PCLK frequency otherwise"

 

My code:

/**
 ******************************************************************************
 * @file 	: main.c
 * @author 	: Johannes S.
 * @brief 	: Main program body
 * @microcontroller	: STM32G030K6T6
 ******************************************************************************
 */

/* Includes ------------------------------------------------------------------*/
#include <main.h>
#include <stdint.h>
#include <StartUp.h>

/* Private typedef -----------------------------------------------------------*/
// Enum for the colors of the RGB LED
typedef enum {
 COLOR_RED,
 COLOR_GREEN,
 COLOR_BLUE,
 COLOR_INVALID
} LED_Color;

// Enum for GPIO Output Control
typedef enum {
 HIGH,
 LOW,
 TOGGLE,
	GPIO_State_INVALID
} GPIO_State;

/* Private function ---------------------------------------------------------*/
void LED_RGB(LED_Color color, uint8_t state);
void GPIO_WritePin(GPIO_TypeDef *GPIOx, uint16_t Pin, uint8_t state);
void Button_1_SetInterrupt(void);
void GPIO_TogglePin(GPIO_TypeDef *GPIOx, uint16_t Pin);


#if !defined(__SOFT_FP__) && defined(__ARM_FP)
 #warning "FPU is not initialized, but the project is compiling for an FPU. Please initialize the FPU before use."
#endif

/**
 * Main function
 */
int main(void)
{
	// Setup Microcontroller
	Flash_Init();			// Set flash wait cycles
	PWR_MODULE_Init();		// Set Internal voltage regulator
	SystemClock_Config();	// Configure Clocks
	GPIO_Init();			// Configure GPIO
	TIM16_us_Tick();		// Configure Timer 16 for delay function

	// Test RGB LED
	LED_RGB(COLOR_RED, HIGH);
	LED_RGB(COLOR_BLUE, HIGH);
	LED_RGB(COLOR_GREEN, HIGH);

	// Configure Button No. 1 as interrupt input
	Button_1_SetInterrupt();

	// Turn red and blue led off - to better recognize flashing green led
	LED_RGB(COLOR_RED, LOW);
	LED_RGB(COLOR_BLUE, LOW);

	// measure_timer_duration();

	// While loop - main loop
	while(1)
	{
		// Test LED blink
		delay_ms(3000);
		LED_RGB(COLOR_GREEN, TOGGLE);
	}
}

/**
 * Function for controlling the RGB LED
 */
void LED_RGB(LED_Color color, GPIO_State state)
{
 uint32_t pin;
 GPIO_TypeDef *LED_GPIO;

 // Color assignment based on Enum
 switch (color) {
 case COLOR_RED:
 pin = LED_RGB_Red_Pin;
 LED_GPIO = LED_RGB_Red_GPIO_Port;
 break;
 case COLOR_GREEN:
 pin = LED_RGB_Green_Pin;
 LED_GPIO = LED_RGB_Green_GPIO_Port;
 break;
 case COLOR_BLUE:
 pin = LED_RGB_Blue_Pin;
 LED_GPIO = LED_RGB_Blue_GPIO_Port;
 break;
 default:
 return; // Invalid color, do nothing
 }

 // Switch on or off based on the status
 switch (state) {
 	case HIGH:
 		GPIO_WritePin(LED_GPIO, pin, 1); // turn LED on
 		break;
 	case LOW:
 		GPIO_WritePin(LED_GPIO, pin, 0); // turn LED off
 		break;
 	case TOGGLE:
 		GPIO_TogglePin(LED_GPIO, pin); // toggle LED
 		break;
 	default:
 		return; // Invalid color, do nothing
 }
}

/**
 * Function for controlling a GPIO output
 */
void GPIO_WritePin(GPIO_TypeDef *GPIOx, uint16_t Pin, uint8_t state) {
 if (state) {
 GPIOx->BSRR = Pin; // set GPIO high (Bit Set Reset Register - BSRR)
 } else {
 GPIOx->BRR = Pin; // set GPIO low (Bit Reset Register - BRR)
 }
}

/**
 * Toggle GPIO Outputs
 */
void GPIO_TogglePin(GPIO_TypeDef *GPIOx, uint16_t Pin) {
	GPIOx->ODR ^= Pin;
}

/**
 * Declare button 1 (PC6) as interrupt
 */
void Button_1_SetInterrupt(void)
{
	// SYSCFG (System Configuration Controller) - Activate clock
	// Required for: “Flag pending interrupts from each interrupt line”
	// See: SYSCFG interrupt line 7 status register (SYSCFG_ITLINE7) - page 196
	RCC->APBENR2 |= RCC_APBENR2_SYSCFGEN; 	// Activate Clock for SYSCFG

	// Connect pin PC6 to EXTI6 (SYSCFG Configuration)
	EXTI->EXTICR[1] = 0x00000000; 		// Reset Register
	EXTI->EXTICR[1] = 0x02 << 16;		// Connect EXTI with PC6
	EXTI->FTSR1 = 0x1UL << 6;			// Interupt triggerd with falling edge

	// Activate interrupt
	// See en.stm32u0-system-extended-interrupt-event-controller-exti.pdf page 6
	// EXTI_FTSR1 output is AND linked with EXTI_IMR1 -> therefore interrupt must be activated here
	EXTI->IMR1 |= EXTI_IMR1_IM6; 	// Unmask interrupt (activate)

	// Activate interrupt and set priority in NVIC (Nested vectored interrupt controller)
	// Configuration for EXTI4_15
	NVIC_SetPriority(EXTI4_15_IRQn, 1); // Set priority to 1 (low)
	NVIC_EnableIRQ(EXTI4_15_IRQn); // Activate interrupt in NVIC
}

/**
 * Interrupt service routine for button 1 (PC6)
 */
void EXTI4_15_IRQHandler(void)
{
	LED_RGB(COLOR_BLUE, TOGGLE);	// Toggle blue LED
	EXTI->FPR1 |= 0x1UL << 6;		// Delete interrupt pending register (otherwise interrupt is triggered again immediately)
}


void TIM16_us_Tick(void)
{
	// Uses PCLK Clock = 16 MHz as source
	// -> According to the data sheet and with the AHB prescaler of 2, this should actually be 8 MHz.
	// However, the input frequency of the timer seems to be independent of the AHB prescaler.

	// Enable TIM16 Clock
	RCC->APBENR2 |= (0x1UL << 17);

	// Set CR1 register
	TIM16->CR1 &= ~TIM_CR1_UIFREMAP;
	TIM16->CR1 |= TIM_CR1_ARPE;

	// Set PSC register
	TIM16->PSC = 15; // Set prescaler to 15 -> 1us task for timer (f_timer = f_pclk / (1+prescaler))

	// Set ARR register
	TIM16->ARR = 0xFFFF; // Maximum value (optional, depending on application)

	// Activate Timer
	//TIM16->CR1 |= TIM_CR1_CEN;
}

void delay_ms(uint16_t ms) {
 // Timer-Setup: Prescaler and ARR are already configured,
 // that the timer counts with 1 µs resolution.
	TIM16->CR1 |= TIM_CR1_CEN; // start Timer
 for (uint16_t i = 0; i < ms; i++) {
 TIM16->CNT = 0; // Reset counter to 0
 TIM16->SR &= ~TIM_SR_UIF; // Reset update flag (UIF)
 //while (TIM16->CNT != 0);	 // Wait until the counter has been set to 0
 //TIM16->CR1 |= TIM_CR1_CEN; // start Timer

 while (TIM16->CNT < 1000); // wait 1000 µs = 1 ms

 //TIM16->CR1 &= ~TIM_CR1_CEN; // stop Timer
 }
 TIM16->CR1 &= ~TIM_CR1_CEN; // stop Timer

 // Edit later so that function is leaner and more accurate
}

/**
 * Function to check timer
 */
void measure_timer_duration(void) {
 TIM16->CNT = 0;
 TIM16->CR1 |= TIM_CR1_CEN;

 for (volatile int i = 0; i < 1000000; ++i); // Short known waiting time

 TIM16->CR1 &= ~TIM_CR1_CEN;
 uint32_t count = TIM16->CNT;
}

 

/**
 ******************************************************************************
 * @author J.Stuermann
 * @file StartUp.h
 * @brief Header file for StartUp.c which sets Register for SMT32G030K6T6 for
 * 		Start Up routine.
 ******************************************************************************
*/

/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Define to prevent recursive inclusion -------------------------------------*/
#ifndef STARTUP_H_
#define STARTUP_H_

// Constants


// Functions
void Flash_Init(void);
void PWR_MODULE_Init(void);
void SystemClock_Config(void);
void GPIO_Init(void);


#endif /* STARTUP_H_ */

 

/**
 ******************************************************************************
 * @author J.Stuermann
 * @file StartUp.h
 * @brief Header file for StartUp.c which sets Register for SMT32G030K6T6 for
 * 		Start Up routine.
 ******************************************************************************
*/

/**
 * Procedure:
 * 1. Set flash wait cycles
 * 2. Set internal voltage regulator
 * 3. Configure System Clock
 * 4. Configure GPIOs
 * 5.
 * 6.
 *
 */

/* Includes ------------------------------------------------------------------*/
#include "StartUp.h"


/* Functions -----------------------------------------------------------------*/

/**
 * Set flash wait cycles
 */
void Flash_Init(void) {
	// Set flash wait cycles based on the system clock frequency.
	// 0 Wait-State for <24 MHz
 // 1 Wait-State für <48 MHz
	// 2 Wait-State für <64 MHz
 FLASH->ACR &= ~0x7UL; // Set Wait-State = 0
}

/**
 * Set internal voltage regulator to “Range 1” -> 1.2 V is required for system clock up to 64 MHz
 */
void PWR_MODULE_Init(void)
{
	// Reset
	PWR->CR1 = 0x00000208;
	// Voltage scaling range - Range 1 - for 64 Mhz System Frequency
	PWR->CR1 = (PWR->CR1 & ~PWR_CR1_VOS_Msk) | PWR_CR1_VOS_0;
	//	Low power run - off
	PWR->CR1 &= ~PWR_CR1_LPR;
}

/**
 * System Clock Configuration
 * System Clock = 16 MHz
 * AHB Clock = 4 MHz
 * APB Clock = 4 MHz
 */
void SystemClock_Config(void)
{
	// 1. Select internal clock (HSI) with a frequency of 16 MHz
	// Clock control register (RCC_CR)
	RCC->CR |= RCC_CR_HSION; 					// turn HSI on
	while (!(RCC->CR & RCC_CR_HSIRDY)); 		// Wait until HSI is stable
	RCC->CR &= ~RCC_CR_HSIDIV_Msk; 				// HSIDIV = 1
	RCC->CR &= ~RCC_CR_PLLON; 					// PLL Clock disable

	// Select HSISYS as System Clock
	// Set APB and AHB prescaler and disable clock output
	// Clock configuration register (RCC_CFGR)
	RCC->CFGR &= RCC_CFGR_SWS_HSISYS; 			// Select HSISYS as System Clock and disable clock output
	RCC->CFGR &= ~RCC_CFGR_PPRE_Msk; 			// Reset APB prescaler = 1
	RCC->CFGR &= ~RCC_CFGR_HPRE_Msk;			// Reset AHB prescaler = 1
	RCC->CFGR |= 0b1001 << RCC_CFGR_HPRE_Pos;	// Set AHB prescaler = 4

	// MCO clock settings:
	// Output: SYSCLK
	// Prescaler: 128 to improve measurement (1000 not possible)
	RCC->CFGR &= ~RCC_CFGR_MCOSEL_Msk; // Reset MCOSEL (clock selector)
	RCC->CFGR |= RCC_CFGR_MCOSEL_0; // choose SYSCLK
	RCC->CFGR &= ~RCC_CFGR_MCOPRE_Msk; // Reset MCOPRE (Prescaler)
	RCC->CFGR |= (0x7UL << RCC_CFGR_MCOPRE_Pos); // Set Prescaler to 128
}

/**
 * Configure GPIOs
 */
void GPIO_Init(void)
{
	// 1. activate GPIO Clocks
	RCC->IOPENR |= RCC_IOPENR_GPIOAEN; // Activate GPIOA clock (for SPI, external interrupts, etc.)
	RCC->IOPENR |= RCC_IOPENR_GPIOBEN; // Activate GPIOB Clock, if required
	RCC->IOPENR |= RCC_IOPENR_GPIOCEN; // Activate GPIOC Clock, if required

	// Declare GPIOA pin PA10 as input - for later external interrupt - switch next to connector
	GPIOA->MODER &= ~GPIO_MODER_MODE10; // Configure PA10 as input
	GPIOA->PUPDR &= ~GPIO_PUPDR_PUPD10; // Neither pull-up nor pull-down for PA10

	// Declare GPIOA pin PC6 as input - for later external interrupt - Additional switch
	GPIOC->MODER &= ~GPIO_MODER_MODE6; // Configure PAC6 as input
	GPIOC->PUPDR &= ~GPIO_PUPDR_PUPD6; 	// Neither pull-up nor pull-down for PC6

	// GPIO pin PB4 as output for RGB LED (red)
	GPIOB->MODER &= ~GPIO_MODER_MODE4; 	// Reset Port
	GPIOB->MODER |= GPIO_MODER_MODE4_0; // Define Pin as Output
	GPIOB->OTYPER &= ~GPIO_OTYPER_OT4;	// Push-Pull output
	GPIOB->OSPEEDR &= ~GPIO_OSPEEDR_OSPEED4; // Reset Speed Setting
	GPIOB->OSPEEDR |= GPIO_OSPEEDR_OSPEED4_1; // Set to High Speed (second fastest)

	// GPIO pin PB6 as output for RGB LED (blue)
	GPIOB->MODER &= ~GPIO_MODER_MODE6; 	// Reset Port
	GPIOB->MODER |= GPIO_MODER_MODE6_0; // Define Pin as Output
	GPIOB->OTYPER &= ~GPIO_OTYPER_OT6;	// Push-Pull output
	GPIOB->OSPEEDR &= ~GPIO_OSPEEDR_OSPEED6; // Reset Speed Setting
	GPIOB->OSPEEDR |= GPIO_OSPEEDR_OSPEED6_1; // Set to High Speed (second fastest)

	// GPIO pin PB5 as output for RGB LED (green)
	GPIOB->MODER &= ~GPIO_MODER_MODE5; 	// Reset Port
	GPIOB->MODER |= GPIO_MODER_MODE5_0; // Define Pin as Output
	GPIOB->OTYPER &= ~GPIO_OTYPER_OT5;	// Push-Pull output
	GPIOB->OSPEEDR &= ~GPIO_OSPEEDR_OSPEED5; // Reset Speed Setting
	GPIOB->OSPEEDR |= GPIO_OSPEEDR_OSPEED5_1; // Set to High Speed (second fastest)

	// Define GPIO pin PA9 as MCO -> MCO - SYSCLK clock output
	GPIOA->MODER &= ~GPIO_MODER_MODE9; 	// Reset Port
	GPIOA->MODER |= GPIO_MODER_MODE9_1; // Define Pin as alternate function mode
	GPIOA->OTYPER &= ~GPIO_OTYPER_OT9;	// Push-Pull output
	GPIOA->OSPEEDR &= ~GPIO_OSPEEDR_OSPEED9; // Reset Speed Setting
	GPIOA->OSPEEDR |= GPIO_OSPEEDR_OSPEED9_1; // Set to High Speed (second fastest)
	GPIOA->AFR[2] &= GPIO_AFRH_AFSEL9; // Reset alternate function register für PA9.
		// The reset value is also directly correct here to select MCO.
		// In the “normal” data sheet there is a table showing which number stands for
		// which alternative function, here AF0 stands for MCO
}
This topic has been closed for replies.
Sarra.SBest answer
ST Employee
Jun 11, 2025 10:31 AM UTC

Hello @JohannesSt , 

This is a known erratum (check errata sheet for the STM32G031 series (ES0487))

TIM16 and TIM17 are unduly clocked by SYSCLK
Description
The timers TIM16 and TIM17 are unduly clocked by SYSCLK instead of being clocked by the timer clock
TIMPCLK. As a consequence, they do not reflect AHB and APB prescaler settings.
The TIM16 and TIM17 are fully functional as long as the SYSCLK-to-PCLK frequency ratio remains smaller than
or equal to four.

Workaround
None.

In your case, since SYSCLK = 16 MHz, TIM16 is being clocked at 16 MHz, which is why your prescaler calculation aligns with this frequency

Edit: ES0486 instead of ES0487 (Corrected by Jan) 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

20 replies

TDK
Jun 3, 2025 12:47 PM UTC

The code is certainly not ideal, but your assumptions are correct. What makes you think it's at the wrong frequency? Start the timer and do a HAL_Delay(100) or something and calculate the CNT before/after to get the frequency. Set prescaler so it doesn't overflow.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate
Jun 3, 2025 2:44 PM UTC

First of all, thank you for your quick response.

 

I would like to further adapt or improve the code. In general, I don't want to use any ready-made libraries, as I am doing this for learning purposes. For this reason, I don't want to use the HAL function.

 

“What makes you think it's at the wrong frequency?” -> The code works as written; the LED flashes every 3 seconds. However, to my understanding, this should not be the case, as the correct prescaler value for the timer would be 3, assuming the input frequency is 4 MHz. However, I have set the prescaler value to 15 – the code works, which surprises me a little and, to be honest, I don't understand.

 

If it helps, I could also upload screenshots of the register values in debug mode, but these also match the values in the code.

waclawek.jan
Super User
Jun 3, 2025 2:51 PM UTC

Hi @JohannesSt ,

At this point I don't have answers to your question, but I am curious: how did you write the original post? In particular, did you emphasise the text in bold manually, or did you use some program to do that for you?

Thanks,

JW

waclawek.jan
Super User
Jun 3, 2025 4:53 PM UTC

OK I think I know what's the problem.

TIMx_PSC is unconditionally preloaded. It means, the value written to it is not used in the internal prescaler, until there is an Update event. Update is basically an overflow; but as you use the timer so that you always stop it before it reaches the overflow, your TIMx_PSC is never applied.

You can test this assertion by using various values for TIMx_PSC, the result should be the same.

I also believe that you compile with all optimizations off, which results in the loopdelay taking longer than just the pure 1000 timer clocks, masking the real timing of the timer.

JW

 

Associate
Jun 4, 2025 7:50 PM UTC

Hi all,

@waclawek.jan i added the following line to update the prescaler value:

// Create Update event to force new values into PSC
TIM16->EGR |= 0x0001;

Afterwards i also checked the register values. The prescaler value is adopted correctly. However, the delay function is still only correct with a prescaler value of 15. I have also entered a prescaler value of 3 which would actually be correct according to the documentation, but here the “blink” frequency is then too fast.

 

So the problem remains. Do you or anyone else have an idea what the problem could be?

MM..1
Super User
Jun 4, 2025 8:16 PM UTC

Maybe order is required , try inspire

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_SYSCFG);
 LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_PWR);

 /* SysTick_IRQn interrupt configuration */
 NVIC_SetPriority(SysTick_IRQn, 3);

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_TIM16_Init();
 /* USER CODE BEGIN 2 */

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 /* HSI configuration and activation */
 LL_RCC_HSI_Enable();
 while(LL_RCC_HSI_IsReady() != 1)
 {
 }

 /* Set AHB prescaler*/
 LL_RCC_SetAHBPrescaler(LL_RCC_SYSCLK_DIV_4);

 /* Sysclk activation on the HSI */
 LL_RCC_SetSysClkSource(LL_RCC_SYS_CLKSOURCE_HSI);
 while(LL_RCC_GetSysClkSource() != LL_RCC_SYS_CLKSOURCE_STATUS_HSI)
 {
 }

 /* Set APB1 prescaler*/
 LL_RCC_SetAPB1Prescaler(LL_RCC_APB1_DIV_1);

 LL_Init1msTick(4000000);

 /* Update CMSIS variable (which can be updated also through SystemCoreClockUpdate function) */
 LL_SetSystemCoreClock(4000000);
}

/**
 * @brief TIM16 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_TIM16_Init(void)
{

 /* USER CODE BEGIN TIM16_Init 0 */

 /* USER CODE END TIM16_Init 0 */

 LL_TIM_InitTypeDef TIM_InitStruct = {0};

 /* Peripheral clock enable */
 LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_TIM16);

 /* TIM16 interrupt Init */
 NVIC_SetPriority(TIM16_IRQn, 0);
 NVIC_EnableIRQ(TIM16_IRQn);

 /* USER CODE BEGIN TIM16_Init 1 */

 /* USER CODE END TIM16_Init 1 */
 TIM_InitStruct.Prescaler = 0;
 TIM_InitStruct.CounterMode = LL_TIM_COUNTERMODE_UP;
 TIM_InitStruct.Autoreload = 65535;
 TIM_InitStruct.ClockDivision = LL_TIM_CLOCKDIVISION_DIV4;
 TIM_InitStruct.RepetitionCounter = 0;
 LL_TIM_Init(TIM16, &TIM_InitStruct);
 LL_TIM_DisableARRPreload(TIM16);
 /* USER CODE BEGIN TIM16_Init 2 */

 /* USER CODE END TIM16_Init 2 */

}
Sarra.SBest answer
ST Employee
Jun 11, 2025 10:31 AM UTC

Hello @JohannesSt , 

This is a known erratum (check errata sheet for the STM32G031 series (ES0487))

TIM16 and TIM17 are unduly clocked by SYSCLK
Description
The timers TIM16 and TIM17 are unduly clocked by SYSCLK instead of being clocked by the timer clock
TIMPCLK. As a consequence, they do not reflect AHB and APB prescaler settings.
The TIM16 and TIM17 are fully functional as long as the SYSCLK-to-PCLK frequency ratio remains smaller than
or equal to four.

Workaround
None.

In your case, since SYSCLK = 16 MHz, TIM16 is being clocked at 16 MHz, which is why your prescaler calculation aligns with this frequency

Edit: ES0486 instead of ES0487 (Corrected by Jan) 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
waclawek.jan
Super User
Jun 11, 2025 1:08 PM UTC

Hi @Sarra.S ,

Thanks for this info. Yes, the good old "read all the documentation, including errata"... Shame on us that we did not spot that. (Btw. technically for 'G030 it's ES0486 rather than ES0487, but that contains the same info).

But, also, the errata say, that rev.Y of the chip fixes this. So the question to @JohannesSt is, does he have rev. Z or rev.Y of the chip?

JW

Associate
Jul 1, 2025 9:22 PM UTC

@Sarra.S @waclawek.jan 

First of all, I would like to apologize for the late reply. I was on vacation and therefore not at my computer.

 

I have revision Z (in errate it says “limitation present, no workaround available”). For me, this means that the corresponding error is present here.

 

I didn't even think of looking in the errata (for a short moment I thought I might have found an unknown error :D).

 

I would like to thank you all, especially @waclawek.jan for the great support and the many suggestions and @Sarra.S for solving the problem. Now at least I know that I wasn't completely *** and can continue practicing :)