Skip to main content
rnd_inglo
Visitor II
Jun 23, 2026 11:33 AM UTC
Solved

STM32G030 ADC channels and VREFINT read 4095 only when battery is connected on 2 boards out of 10

I am using an STM32G030C8T6.

I have 10 boards built from the same PCB design and BOM. All boards use the same firmware.

8 boards work correctly, but 2 boards show abnormal ADC readings.

ADC channels used:

  • PA1 = ADC_IN1

  • PA5 = ADC_IN5

  • PA6 = ADC_IN6

  • PB0 = ADC_IN8

  • PB1 = ADC_IN9

  • PB2 = ADC_IN10

  • VREFINT

ADC configuration:

  • 12-bit resolution

  • Continuous conversion enabled

  • Scan conversion enabled

  • DMA circular mode

  • Sampling time = 160.5 cycles

  • VREFINT included in the scan sequence

Problem:

On the failing boards, when the battery is connected, some ADC channels become 4095.

Example:

LOAD_I_ADC = 4095
PV_A_ADC = 4095
BAT_A_ADC = 4095
VREFINT_ADC = 4095

Other channels still show valid values.

Measured VDDA:

  • Battery disconnected: 3.32V

  • Battery connected: 3.33V

To isolate the issue, I created a separate test project using only the following:

  • ADC_IN9 (PB1)

  • VREFINT

Results with battery disconnected:

adcBuf[0] = 1415
adcBuf[1] = 1518

These values appear normal.

I then created another test project using only VREFINT with a single ADC conversion to determine whether the issue is related to channel interaction or an external analog circuit.

My questions:

  1. Can ADC sample-and-hold capacitor effects or source impedance issues cause VREFINT to read 4095?

  2. Can an external analog input force VREFINT conversions to become saturated?

  3. Has anyone seen ADC channels and VREFINT become 4095 only when a battery is connected while VDDA remains stable at 3.33 V?

  4. What additional measurements or tests would you recommend?

Any suggestions would be appreciated.

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jun 23, 2026 11:38 AM UTC

Hello, 

Need first to check your PCB. Probably there are some soldering joints issue.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jun 23, 2026 11:38 AM UTC

Hello, 

Need first to check your PCB. Probably there are some soldering joints issue.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.