Associate II
Aug 5, 2021 2:49 PM UTC
Solved
STM32G0 Variable square wave generation
- 12 replies
- 4762 views
Hi all, I'm using a NUCLEO-G071RB board and I simply want to generate a variable frequency square wave. I started from project TIM_OCToggle found on the examples.
My problem is that TIM1 channel 1 has a fixed frequency and even if I change it through the sConfigOC struct with HAL functions, and I see changes in htim1->Instance registers after my function SetOutputFrequency(), nothing seems to happen on the ouput PA8, I see only some periods ON or OFF with the oscilloscope. Where are my errors? Is there a simple way to do what I need without using HAL libraries (portability and readability doesn't walk together...) ? Thanks in advance, Emanuele.