Skip to main content
Visitor II
Sep 6, 2025 4:26 PM UTC
Question

STM32G0 USBSEL documentation bug?

Hello, I'm working with a STM32G0B0CE part.  I believe that the TRM definitions for RCC_CCIPR2->USBSEL are incorrect.

I was having trouble with USB, seemingly related to clock selection.  I noticed in the LL HAL headers the following:

#define LL_RCC_USB_CLKSOURCE_HSE RCC_CCIPR2_USBSEL_0 /*!< PLL clock used as USB clock source */
#define LL_RCC_USB_CLKSOURCE_PLL RCC_CCIPR2_USBSEL_1 /*!< PLL clock used as USB clock source */
#define RCC_CCIPR2_USBSEL_Pos (12U)
#define RCC_CCIPR2_USBSEL_Msk (0x3UL << RCC_CCIPR2_USBSEL_Pos) /*!< 0x00003000 */
#define RCC_CCIPR2_USBSEL RCC_CCIPR2_USBSEL_Msk
#define RCC_CCIPR2_USBSEL_0 (0x1UL << RCC_CCIPR2_USBSEL_Pos) /*!< 0x00001000 */
#define RCC_CCIPR2_USBSEL_1 (0x2UL << RCC_CCIPR2_USBSEL_Pos) /*!< 0x00002000 */
 

This seems to indicate that USBSEL should be 0x2 for PLL and 0x1 for HSE.

RM0454 Rev 5 Page 165 indicates that 0x1 is PLL and 0x2 is HSE.

I have confirmed that USB is functional on my board when setting USBSEL to 0x2 and is not functional when using 0x1, so I believe that the HAL definitions are correct and the documentation is wrong.

I'm using an 8 MHz external oscillator and generating a 48MHz output from the PLL, so it is expected that the HSE should not work as a USB clock source.



This topic has been closed for replies.

1 reply

ST Technical Moderator
Sep 7, 2025 6:02 PM UTC

Hello @DFurie and welcome to the Community,

You are right, the register RCC_CCIPR2 contains incorrect values on the USBSEL field.

An internal ticket (ID: 217013) is submitted to push the update of the reference manual RM0454 with the correct reference :

  • 01: HSE
  • 10: PLLQCLK

Thank you for your contribution and for rising this up.

PS: Ticket (ID: 217013) is only for reference, not available outside of ST.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks