Skip to main content
sagar_bn
Associate II
April 9, 2023
Solved

STM32G0 series Programmers & Debuggers

Hello All,

I'm new to ST products. We are using STM32G041F8P6 in our project. This IC will be programmed through I2C/USART and there's no JTAG available for this chip. Please suggest some low-cost programmers/debuggers.

Thank you

This topic has been closed for replies.
Danish1
Danish1Best answer
Lead III
April 9, 2023

Jtag would use too many pins. Instead you have to use SWDIO and SWCLK so you need a debugger that supports that protocol. You should also wire up Reset.

ST-Link is a good choice.

I think Olimex have a solution as well.

If you already have a Nucleo board, you might be able to repurpose the built-in STLink for your prototypes.

5 replies

Danish1
Danish1Best answer
Lead III
April 9, 2023

Jtag would use too many pins. Instead you have to use SWDIO and SWCLK so you need a debugger that supports that protocol. You should also wire up Reset.

ST-Link is a good choice.

I think Olimex have a solution as well.

If you already have a Nucleo board, you might be able to repurpose the built-in STLink for your prototypes.

sagar_bn
sagar_bnAuthor
Associate II
April 10, 2023

Hi Danish,

Thanks for the reply. I have 2 Queries, please clear my doubts:

  1. Can I program the internal Flash using Serial Wire Debug Interface
  2. If USART is used for programming, Is debugger required ? Can I directly send the USART commands through my PC (USB to RS232 and then RS232 to USART) to the UART pins of the board.
Danish1
Lead III
April 11, 2023
  1. Yes. That (or full-blown JTAG) is how I program all my stm32. And that’s how people program the stm32 Nucleo demo boards.
  2. A debugger isn’t required if you’re using one of the serial interfaces supported by the bootloader that’s built into your stm32. You will need a jumper on the BOOT0 pin to select between your code and the bootloader. “TTL-level�? USB-to-serial adapters exist. But you lose the ability to interactively debug your code; for me that would be a huge loss.
sagar_bn
sagar_bnAuthor
Associate II
April 11, 2023

Hi Danish,

Thanks for the very good explaination.

Can u please give little more info on Boot0 pin - is it only to select booting from system flash, user flash, or embedded SRAM. Does this Boot0 pin selection to be taken care if we are programming through UART/I2C ? Is there any pin settings to be done to program from UART/I2C ?

Danish1
Lead III
April 11, 2023