Skip to main content
TSu.1
Associate II
Apr 17, 2025 12:09 PM UTC
Solved

STM32G0 crashes into system memory bootloader everytime during debug

The codebase is generated by CubeMX and now I'm facing issues during debug.

debug method is SWD using ST-LINK V2.

In debug mode, after resume fron HAL_Init(); , the code will crashed into system memory zone and have no debug information.

Break at address "0x1fff12ca" with no debug information available, or outside of program code.

the location of the address varies around 0x1fffxxxx sometimes.

to be exact, the crash will happen when:

Initialize the IWDG

Using Flash R/W Operation

Start Timer (But not Init)

In STM32G031, 0x1fff12ca is located at system memory area where it houses the factory bootloader.

What confuses me is, I have another code project that has basically the same start up code at main() but it works just fine (in another STM32G031, and hardware connection is the same regarding BOOT0 pin). Tried Clean project and rebuild, restart IDE and change optimization, changing minimum heap and stack, absolutely no help whatsoever. I have not try to load the codes to another STM32G031 yet but what will be the possible reason that causes this?

This topic has been closed for replies.
TDK
TDKBest answer
Apr 17, 2025 6:07 PM UTC

Correct. It checks at power on. If firmware is loaded, the flash will not be detected as empty.

"If you feel a post has answered your question, please click ""Accept as Solution""."

10 replies

TDK
Apr 17, 2025 12:43 PM UTC

Is this a custom board? If so, is BOOT0 held low? That is the most likely issue.

Is SCB->VTOR set up correctly? Generally should be pointing at 0x08000000.

IWDG in general does not stop during debug and may be resetting. Bootloader may be getting loaded if option bytes or BOOTx pins are not set correctly.

"If you feel a post has answered your question, please click ""Accept as Solution""."
TSu.1
TSu.1Author
Associate II
Apr 17, 2025 1:01 PM UTC

Yes both are custom board and the BOOT0 pin is technically 'floating' when SWCLK is not connected. No external pull-down resistor. 

usually for a brand new chip it should be fine without further setting ob and BOOTx pins, at least I have not encountered this for the last few other STM32G031s.

how do I check SCB-VTOR in STM32CubeIDE?

TDK
Apr 17, 2025 1:10 PM UTC

BOOT0 needs held low during startup to boot into user flash.

Alternatively, you can modify option bytes such that it ignored the BOOT0 pin and always boots there.

> usually for a brand new chip it should be fine without further setting ob and BOOTx pins

This is not correct. A floating BOOTx pin is a common cause of issues. There isn't a chip I know of where the value is ignored by default when the flash is not empty.

 

Edit: You might be correct here for the STM32G0x1 in particular. Seems like BOOTx pin value is not used by default. In which case I'd check option bytes to see how it's set up to boot.

"If you feel a post has answered your question, please click ""Accept as Solution""."