Skip to main content
Associate III
September 5, 2024
Solved

STM32G0 bootloader usart loop

Hi,

I am using built-in usart bootloader on stm32g0. And I am also using the same usart for communication in my user app. I enabled the bootloader via boot option bits. When I start the debug session, I can see the flow stepping over through the program flow, going over HAL_Init(), SystemClock_Config(),  MX_GPIO_Init() and MX_USART1_UART_Init(), and then the program flow comes to my first "HAL_UART_Receive(..." function. 

It is at this function that the program jumps to the Bootloader and the bootloader starts to respond to my uasrt commands. After I exit the bootloader, via the "Go command(I use address 0x08000000)", the program flow stops at breakpoint I have at "HAL_Init()" and then when I step over again, I see that as soon as I hit the "HAL_UART_Receive(..." function again, it goes back into bootloader.

 

So, my thinking now is that after I exit the bootloader, I should modify the boot bit (nBOOT0) in my user code, to disable it and then enabling it again via the uart command later, if i want to return to bootloader?

int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_USART1_UART_Init();
 //MX_ADC1_Init();
 /* USER CODE BEGIN 2 */
 char tmp[1]; //Dummy variable for next line HAL uart receive function.
 HAL_UART_Receive(&huart1, tmp, 1, 500);
 //cha...

 

 

 

 

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
September 5, 2024

RM0444 Rev 5 / Sections 2.5 Boot configuration and 3.4.2 FLASH option byte programming.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

6 replies

mƎALLEm
ST Technical Moderator
September 5, 2024

Hello @KlemenPfce 

If you configure the option bytes to Jump to the system memory and you didn't changed it to jump to the Flash memory (to run your application), indeed, the MCU keeps  running the system memory. So you need to restore the default option bytes boot config to jump to the Flash memory and, if needed, modify it again for system memory to execute bootloader program. Make sure you make a system reset after each change to let the MCU reading these new values at startup.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Associate III
September 5, 2024

Yes, so I need to modify option bytes inside my code. But I cant find info on how to do it. Is there an AN or RM where this process is described?

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
September 5, 2024

RM0444 Rev 5 / Sections 2.5 Boot configuration and 3.4.2 FLASH option byte programming.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
BarryWhit
Lead
September 5, 2024

If you're using a really low-pin count package, perhaps this thread is relevant.

AKA "Life gets interesting when NRST and the UART share a pin".

"- If someone's post helped resolve your issue, please thank them by clicking ""Accept as Solution"".- Please post an update with details once you've solved your issue. Your experience may help others."