STM32F7xx is a 216 MHz ARM MCU But I Can Not Generate Even 0.5 microsecond Timer Interrupt?
Hi,
//In my project i want to use 0.5 us (500 nanosecond) timer interrupt counter.
//The MCUs max speed is 216 MHz. To get 200 MHz clock frequency, My OSC and CLOCK Settings are
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;
HAL_StatusTypeDef ret = HAL_OK;
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 4;
RCC_OscInitStruct.PLL.PLLN = 192;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 8;
ret = HAL_RCC_OscConfig(&RCC_OscInitStruct);
if(ret != HAL_OK)
{
while(1){;}
}
ret = HAL_PWREx_EnableOverDrive();
if(ret != HAL_OK)
{
while(1){;}
}
RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2);
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
ret = HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_7);
if(ret != HAL_OK)
{
while(1){;}
}
}
//and
//TIMER Settings for 5 us interrupt output
TIM_HandleTypeDef htim2 = {
.Instance = TIM2};
__HAL_RCC_TIM2_CLK_ENABLE();
htim9.Init.Prescaler = 99;
htim9.Init.CounterMode = TIM_COUNTERMODE_UP;
htim9.Init.Period = 9;
htim9.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim9.Init.RepetitionCounter = 0x00;
HAL_TIM_Base_Init(&htim2);
HAL_TIM_Base_Start_IT(&htim2);
HAL_NVIC_SetPriority(TIM2_IRQn, 0x00, 0x00);
HAL_NVIC_EnableIRQ(TIM2_IRQn);
//then for 1 second LED blink using 100.000 counter variable in following function;
void TIM2_IRQHandler()
{
second++;
HAL_TIM_IRQHandler(&htim2);
}
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
if(second == 90.000)
{
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_7, GPIO_PIN_SET);
}
if(second == 100.000)
{
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_7, GPIO_PIN_RESET);
second = 0;
}
}
Led blinks 1 time in one second. Ok.
//***But if I decrease the division factor to get 0.5 us -500 nanosecond- changing counter variable = 1.000.000 to get 1 second LED blink***
htim9.Init.Prescaler = 9;
htim9.Init.CounterMode = TIM_COUNTERMODE_UP;
htim9.Init.Period = 9;
//It slows down that around 2 sec/blink!!! and even if i continue to decrease Prescaler = under 9 or Period = under 9 the speed of LED blinking doesnt chance!!!
//I wisited hundreds of web pages and i read toushands of pages of documents but couldnt find any useful description or solution! I just found a trick in a document DM00224583 (RCC dedicated clocks configuration register (RCC_DCKCFGRx)) about APB1 and APB2 that their division must be 1 to conduct high speed frequency, but my setings are already same with that division 1!!! Since we will never be able to use it, why it is so fast this much 216 MHz?
//Could you help me how to generate 0.5 us interrupt with 216 MHz High speed MCU STM32F7xx????