Skip to main content
A3_it
Associate III
March 10, 2020
Question

STM32F779NI internal ADC accuracy

  • March 10, 2020
  • 9 replies
  • 1221 views

I am using internal ADC of STM32F779NI connected to LMT86 Temperature sensor.

Vref is 3.3v and ADC resolution used is 10-bit.

The problem is there is always a difference with the expected ADC and the actual ADC for a given voltage. This difference is lower at a lower voltage and increases with higher voltage.

E.g At 1505 mv, calculated ADC is 467, but the generated ADC value is 458; difference of 9.

At 3023 mv, calculated ADC is 938 but the generated ADC value is 922; difference of 16.

Find below some more readings:

Input Voltage Generated ADC Value Calculated/Expected ADC value

(mv)

277 86 86

323 99 100

1806 552 561

Is the difference is because of some internal conversion error or is there anything missing in ADC settings? What could be the source of error and suggestion to resolve/workaround?

This topic has been closed for replies.

9 replies

berendi
Principal
March 10, 2020

Verify that Vref+ <= Vdda <= Vdd during the conversion.

Ozone
Principal
March 10, 2020

Not sure what LM86 sensor you speak about, the one I found has a I2C interface.

Assuming a proper Vref and Vdda/Vref relation (as berendi noted), an insufficient sensor output impedance could cause such problems as well.

berendi
Principal
March 10, 2020

LM86 has a digital I2C/SMBUS interface.

This question is about the LMT86 which has analog output.

Ozone
Principal
March 10, 2020

I'm pretty sure the original post said "LM86T".

Retrospective editing destroys the conversation's logical sequence.

waclawek.jan
Super User
March 10, 2020

What a great idea, TI, to produce parts with different characteristics under such a similar name.

From the DS:

Output drive T A = T J = 25°C –50 50 µA

I'd say, this may be a case of inadequate sampling time.

JW

Ozone
Principal
March 10, 2020

> I'd say, this may be a case of inadequate sampling time.

Supposedly true.

For 50uA max, one would need quite a long sampling time.

A buffer opamp would be a solution.

A3_it
A3_itAuthor
Associate III
March 11, 2020

Thanks everyone for your prompt reply and helpful suggestions.

The problem was with Vref+ only. Calculated ADC was with Vref = 3.3v.

But actually the Vref was not 3.3v. It is 3.353v in one board and 3.360v in another board.

Calculating ADC with these Vref value matches with generated ADC value.

Thanks