Skip to main content
Associate
January 18, 2024
Question

stm32f779i -EVAL IAP

  • January 18, 2024
  • 2 replies
  • 1150 views

Hello experts,

I am using stm32f779I - EVAL evaluation kit, am trying to implement LWIP IAP on this board for that I have used example code from the repository C:\Users\Aravind\STM32Cube\Repository\STM32Cube_FW_F7_V1.17.0\Projects\STM32F769I_EVAL\Applications\LwIP\LwIP_IAP and binary file of application availabe in same repository, it is working fine as the binary file says four LEDS toggles, it is toggling.

 I have written my own application LED2 toggle with flash base address 0x08020000 and vector offset = 0x20000 and generated the binary file using STM CUBE IDE and tried to run, it is getting into not valid stack address (LED 3 is getting on ). The other way I generated the binary file using keil and loaded, now the stack address is getting valid but my application is not working as expected (LED2 is not toggling). I have attached the IAP code below which is working fine with binary file from repository but same IAP is getting into not valid stack address with my binary file.

if (((*(__IO uint32_t*)USER_FLASH_FIRST_PAGE_ADDRESS) & 0x2FFE0000 ) == 0x20000000)
{
/* Jump to user application */
JumpAddress = *(__IO uint32_t*) (USER_FLASH_FIRST_PAGE_ADDRESS + 4);
Jump_To_Application = (pFunction) JumpAddress;
/* Initialize user application's Stack Pointer */
__set_MSP(*(__IO uint32_t*) USER_FLASH_FIRST_PAGE_ADDRESS);
Jump_To_Application();
/* do nothing */
while(1);
}
else
{/* Otherwise, do nothing */
/* LED3 (RED) ON to indicate bad software (when not valid stack address) */
BSP_LED_Init(LED3);
BSP_LED_On(LED3);
/* do nothing */
while(1);
}

Please let me know what am I missing.

Thanks & Regards

Aravind K

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
January 18, 2024

Get serial output working so you can output useful diagnostic information. 

Check your binary, what are the initial two 32-bit words there.

What do you set the initial stack value too

 Check startup.s and the Linker script .ld file.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Aravind1Author
Associate
January 19, 2024

Hello Tesla DeLorean,

Thanks for the reply,

Check your binary, what are the initial two 32-bit words there.

20080000 080207E5  This is the first two 32 bit words which is not going to satisfy the condition in IAP code.

What do you set the initial stack value too

You mean the vector offset, I set the vector offset with 0x20000.

 Check startup.s and the Linker script .ld file.

 I am sharing the linker file and startup.s below, Can you please check if I am making any mistake.

/*
******************************************************************************
**
** @file : LinkerScript.ld
**
** @author : Auto-generated by STM32CubeIDE
**
** Abstract : Linker script for STM32F779I-EVAL Board embedding STM32F779NIHx Device from stm32f7 series
** 2048KBytes FLASH
** 512KBytes RAM
**
** Set heap size, stack size and stack location according
** to application requirements.
**
** Set memory bank area and size if external memory is used
**
** Target : STMicroelectronics STM32
**
** Distribution: The file is distributed as is, without any warranty
** of any kind.
**
******************************************************************************
** @attention
**
** Copyright (c) 2024 STMicroelectronics.
** All rights reserved.
**
** This software is licensed under terms that can be found in the LICENSE file
** in the root directory of this software component.
** If no LICENSE file comes with this software, it is provided AS-IS.
**
******************************************************************************
*/

/* Entry Point */
ENTRY(Reset_Handler)

/* Highest address of the user mode stack */
_estack = ORIGIN(RAM) + LENGTH(RAM); /* end of "RAM" Ram type memory */

_Min_Heap_Size = 0x2000; /* required amount of heap */
_Min_Stack_Size = 0x4000; /* required amount of stack */

/* Memories definition */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 512K
FLASH (rx) : ORIGIN = 0x8020000, LENGTH = 2048K
}

/* Sections */
SECTIONS
{
/* The startup code into "FLASH" Rom type memory */
.isr_vector :
{
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} >FLASH

/* The program code and other data into "FLASH" Rom type memory */
.text :
{
. = ALIGN(4);
*(.text) /* .text sections (code) */
*(.text*) /* .text* sections (code) */
*(.glue_7) /* glue arm to thumb code */
*(.glue_7t) /* glue thumb to arm code */
*(.eh_frame)

KEEP (*(.init))
KEEP (*(.fini))

. = ALIGN(4);
_etext = .; /* define a global symbols at end of code */
} >FLASH

/* Constant data into "FLASH" Rom type memory */
.rodata :
{
. = ALIGN(4);
*(.rodata) /* .rodata sections (constants, strings, etc.) */
*(.rodata*) /* .rodata* sections (constants, strings, etc.) */
. = ALIGN(4);
} >FLASH

.ARM.extab : {
. = ALIGN(4);
*(.ARM.extab* .gnu.linkonce.armextab.*)
. = ALIGN(4);
} >FLASH

.ARM : {
. = ALIGN(4);
__exidx_start = .;
*(.ARM.exidx*)
__exidx_end = .;
. = ALIGN(4);
} >FLASH

.preinit_array :
{
. = ALIGN(4);
PROVIDE_HIDDEN (__preinit_array_start = .);
KEEP (*(.preinit_array*))
PROVIDE_HIDDEN (__preinit_array_end = .);
. = ALIGN(4);
} >FLASH

.init_array :
{
. = ALIGN(4);
PROVIDE_HIDDEN (__init_array_start = .);
KEEP (*(SORT(.init_array.*)))
KEEP (*(.init_array*))
PROVIDE_HIDDEN (__init_array_end = .);
. = ALIGN(4);
} >FLASH

.fini_array :
{
. = ALIGN(4);
PROVIDE_HIDDEN (__fini_array_start = .);
KEEP (*(SORT(.fini_array.*)))
KEEP (*(.fini_array*))
PROVIDE_HIDDEN (__fini_array_end = .);
. = ALIGN(4);
} >FLASH

/* Used by the startup to initialize data */
_sidata = LOADADDR(.data);

/* Initialized data sections into "RAM" Ram type memory */
.data :
{
. = ALIGN(4);
_sdata = .; /* create a global symbol at data start */
*(.data) /* .data sections */
*(.data*) /* .data* sections */
*(.RamFunc) /* .RamFunc sections */
*(.RamFunc*) /* .RamFunc* sections */

. = ALIGN(4);
_edata = .; /* define a global symbol at data end */

} >RAM AT> FLASH

/* Uninitialized data section into "RAM" Ram type memory */
. = ALIGN(4);
.bss :
{
/* This is used by the startup in order to initialize the .bss section */
_sbss = .; /* define a global symbol at bss start */
__bss_start__ = _sbss;
*(.bss)
*(.bss*)
*(COMMON)

. = ALIGN(4);
_ebss = .; /* define a global symbol at bss end */
__bss_end__ = _ebss;
} >RAM

/* User_heap_stack section, used to check that there is enough "RAM" Ram type memory left */
._user_heap_stack :
{
. = ALIGN(8);
PROVIDE ( end = . );
PROVIDE ( _end = . );
. = . + _Min_Heap_Size;
. = . + _Min_Stack_Size;
. = ALIGN(8);
} >RAM

/* Remove information from the compiler libraries */
/DISCARD/ :
{
libc.a ( * )
libm.a ( * )
libgcc.a ( * )
}

.ARM.attributes 0 : { *(.ARM.attributes) }
}

 ***********************************************************

/**

 

Here the startup.s starts
******************************************************************************
* @file startup_stm32f779xx.s
* @author MCD Application Team
* @brief STM32F779xx Devices vector table for GCC based toolchain.
* This module performs:
* - Set the initial SP
* - Set the initial PC == Reset_Handler,
* - Set the vector table entries with the exceptions ISR address
* - Branches to main in the C library (which eventually
* calls main()).
* After Reset the Cortex-M7 processor is in Thread mode,
* priority is Privileged, and the Stack is set to Main.
******************************************************************************
* @attention
*
* Copyright (c) 2016 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/

.syntax unified
.cpu cortex-m7
.fpu softvfp
.thumb

.global g_pfnVectors
.global Default_Handler

/* start address for the initialization values of the .data section.
defined in linker script */
.word _sidata
/* start address for the .data section. defined in linker script */
.word _sdata
/* end address for the .data section. defined in linker script */
.word _edata
/* start address for the .bss section. defined in linker script */
.word _sbss
/* end address for the .bss section. defined in linker script */
.word _ebss
/* stack used for SystemInit_ExtMemCtl; always internal RAM used */

/**
* @brief This is the code that gets called when the processor first
* starts execution following a reset event. Only the absolutely
* necessary set is performed, after which the application
* supplied main() routine is called.
* @PAram None
* @retval : None
*/

.section .text.Reset_Handler
.weak Reset_Handler
.type Reset_Handler, %function
Reset_Handler:
ldr sp, =_estack /* set stack pointer */

/* Copy the data segment initializers from flash to SRAM */
ldr r0, =_sdata
ldr r1, =_edata
ldr r2, =_sidata
movs r3, #0
b LoopCopyDataInit

CopyDataInit:
ldr r4, [r2, r3]
str r4, [r0, r3]
adds r3, r3, #4

LoopCopyDataInit:
adds r4, r0, r3
cmp r4, r1
bcc CopyDataInit

/* Zero fill the bss segment. */
ldr r2, =_sbss
ldr r4, =_ebss
movs r3, #0
b LoopFillZerobss

FillZerobss:
str r3, [r2]
adds r2, r2, #4

LoopFillZerobss:
cmp r2, r4
bcc FillZerobss

/* Call the clock system intitialization function.*/
bl SystemInit
/* Call static constructors */
bl __libc_init_array
/* Call the application's entry point.*/
bl main
bx lr
.size Reset_Handler, .-Reset_Handler

/**
* @brief This is the code that gets called when the processor receives an
* unexpected interrupt. This simply enters an infinite loop, preserving
* the system state for examination by a debugger.
* @PAram None
* @retval None
*/
.section .text.Default_Handler,"ax",%progbits
Default_Handler:
Infinite_Loop:
b Infinite_Loop
.size Default_Handler, .-Default_Handler
/******************************************************************************
*
* The minimal vector table for a Cortex M7. Note that the proper constructs
* must be placed on this to ensure that it ends up at physical address
* 0x0000.0000.
*
*******************************************************************************/
.section .isr_vector,"a",%progbits
.type g_pfnVectors, %object
.size g_pfnVectors, .-g_pfnVectors


g_pfnVectors:
.word _estack
.word Reset_Handler

.word NMI_Handler
.word HardFault_Handler
.word MemManage_Handler
.word BusFault_Handler
.word UsageFault_Handler
.word 0
.word 0
.word 0
.word 0
.word SVC_Handler
.word DebugMon_Handler
.word 0
.word PendSV_Handler
.word SysTick_Handler

/* External Interrupts */
.word WWDG_IRQHandler /* Window WatchDog */
.word PVD_IRQHandler /* PVD through EXTI Line detection */
.word TAMP_STAMP_IRQHandler /* Tamper and TimeStamps through the EXTI line */
.word RTC_WKUP_IRQHandler /* RTC Wakeup through the EXTI line */
.word FLASH_IRQHandler /* FLASH */
.word RCC_IRQHandler /* RCC */
.word EXTI0_IRQHandler /* EXTI Line0 */
.word EXTI1_IRQHandler /* EXTI Line1 */
.word EXTI2_IRQHandler /* EXTI Line2 */
.word EXTI3_IRQHandler /* EXTI Line3 */
.word EXTI4_IRQHandler /* EXTI Line4 */
.word DMA1_Stream0_IRQHandler /* DMA1 Stream 0 */
.word DMA1_Stream1_IRQHandler /* DMA1 Stream 1 */
.word DMA1_Stream2_IRQHandler /* DMA1 Stream 2 */
.word DMA1_Stream3_IRQHandler /* DMA1 Stream 3 */
.word DMA1_Stream4_IRQHandler /* DMA1 Stream 4 */
.word DMA1_Stream5_IRQHandler /* DMA1 Stream 5 */
.word DMA1_Stream6_IRQHandler /* DMA1 Stream 6 */
.word ADC_IRQHandler /* ADC1, ADC2 and ADC3s */
.word CAN1_TX_IRQHandler /* CAN1 TX */
.word CAN1_RX0_IRQHandler /* CAN1 RX0 */
.word CAN1_RX1_IRQHandler /* CAN1 RX1 */
.word CAN1_SCE_IRQHandler /* CAN1 SCE */
.word EXTI9_5_IRQHandler /* External Line[9:5]s */
.word TIM1_BRK_TIM9_IRQHandler /* TIM1 Break and TIM9 */
.word TIM1_UP_TIM10_IRQHandler /* TIM1 Update and TIM10 */
.word TIM1_TRG_COM_TIM11_IRQHandler /* TIM1 Trigger and Commutation and TIM11 */
.word TIM1_CC_IRQHandler /* TIM1 Capture Compare */
.word TIM2_IRQHandler /* TIM2 */
.word TIM3_IRQHandler /* TIM3 */
.word TIM4_IRQHandler /* TIM4 */
.word I2C1_EV_IRQHandler /* I2C1 Event */
.word I2C1_ER_IRQHandler /* I2C1 Error */
.word I2C2_EV_IRQHandler /* I2C2 Event */
.word I2C2_ER_IRQHandler /* I2C2 Error */
.word SPI1_IRQHandler /* SPI1 */
.word SPI2_IRQHandler /* SPI2 */
.word USART1_IRQHandler /* USART1 */
.word USART2_IRQHandler /* USART2 */
.word USART3_IRQHandler /* USART3 */
.word EXTI15_10_IRQHandler /* External Line[15:10]s */
.word RTC_Alarm_IRQHandler /* RTC Alarm (A and B) through EXTI Line */
.word OTG_FS_WKUP_IRQHandler /* USB OTG FS Wakeup through EXTI line */
.word TIM8_BRK_TIM12_IRQHandler /* TIM8 Break and TIM12 */
.word TIM8_UP_TIM13_IRQHandler /* TIM8 Update and TIM13 */
.word TIM8_TRG_COM_TIM14_IRQHandler /* TIM8 Trigger and Commutation and TIM14 */
.word TIM8_CC_IRQHandler /* TIM8 Capture Compare */
.word DMA1_Stream7_IRQHandler /* DMA1 Stream7 */
.word FMC_IRQHandler /* FMC */
.word SDMMC1_IRQHandler /* SDMMC1 */
.word TIM5_IRQHandler /* TIM5 */
.word SPI3_IRQHandler /* SPI3 */
.word UART4_IRQHandler /* UART4 */
.word UART5_IRQHandler /* UART5 */
.word TIM6_DAC_IRQHandler /* TIM6 and DAC1&2 underrun errors */
.word TIM7_IRQHandler /* TIM7 */
.word DMA2_Stream0_IRQHandler /* DMA2 Stream 0 */
.word DMA2_Stream1_IRQHandler /* DMA2 Stream 1 */
.word DMA2_Stream2_IRQHandler /* DMA2 Stream 2 */
.word DMA2_Stream3_IRQHandler /* DMA2 Stream 3 */
.word DMA2_Stream4_IRQHandler /* DMA2 Stream 4 */
.word ETH_IRQHandler /* Ethernet */
.word ETH_WKUP_IRQHandler /* Ethernet Wakeup through EXTI line */
.word CAN2_TX_IRQHandler /* CAN2 TX */
.word CAN2_RX0_IRQHandler /* CAN2 RX0 */
.word CAN2_RX1_IRQHandler /* CAN2 RX1 */
.word CAN2_SCE_IRQHandler /* CAN2 SCE */
.word OTG_FS_IRQHandler /* USB OTG FS */
.word DMA2_Stream5_IRQHandler /* DMA2 Stream 5 */
.word DMA2_Stream6_IRQHandler /* DMA2 Stream 6 */
.word DMA2_Stream7_IRQHandler /* DMA2 Stream 7 */
.word USART6_IRQHandler /* USART6 */
.word I2C3_EV_IRQHandler /* I2C3 event */
.word I2C3_ER_IRQHandler /* I2C3 error */
.word OTG_HS_EP1_OUT_IRQHandler /* USB OTG HS End Point 1 Out */
.word OTG_HS_EP1_IN_IRQHandler /* USB OTG HS End Point 1 In */
.word OTG_HS_WKUP_IRQHandler /* USB OTG HS Wakeup through EXTI */
.word OTG_HS_IRQHandler /* USB OTG HS */
.word DCMI_IRQHandler /* DCMI */
.word CRYP_IRQHandler /* Crypto */
.word HASH_RNG_IRQHandler /* Hash and Rng */
.word FPU_IRQHandler /* FPU */
.word UART7_IRQHandler /* UART7 */
.word UART8_IRQHandler /* UART8 */
.word SPI4_IRQHandler /* SPI4 */
.word SPI5_IRQHandler /* SPI5 */
.word SPI6_IRQHandler /* SPI6 */
.word SAI1_IRQHandler /* SAI1 */
.word LTDC_IRQHandler /* LTDC */
.word LTDC_ER_IRQHandler /* LTDC error */
.word DMA2D_IRQHandler /* DMA2D */
.word SAI2_IRQHandler /* SAI2 */
.word QUADSPI_IRQHandler /* QUADSPI */
.word LPTIM1_IRQHandler /* LPTIM1 */
.word CEC_IRQHandler /* HDMI_CEC */
.word I2C4_EV_IRQHandler /* I2C4 Event */
.word I2C4_ER_IRQHandler /* I2C4 Error */
.word SPDIF_RX_IRQHandler /* SPDIF_RX */
.word DSI_IRQHandler /* DSI */
.word DFSDM1_FLT0_IRQHandler /* DFSDM1 Filter 0 global Interrupt */
.word DFSDM1_FLT1_IRQHandler /* DFSDM1 Filter 1 global Interrupt */
.word DFSDM1_FLT2_IRQHandler /* DFSDM1 Filter 2 global Interrupt */
.word DFSDM1_FLT3_IRQHandler /* DFSDM1 Filter 3 global Interrupt */
.word SDMMC2_IRQHandler /* SDMMC2 */
.word CAN3_TX_IRQHandler /* CAN3 TX */
.word CAN3_RX0_IRQHandler /* CAN3 RX0 */
.word CAN3_RX1_IRQHandler /* CAN3 RX1 */
.word CAN3_SCE_IRQHandler /* CAN3 SCE */
.word JPEG_IRQHandler /* JPEG */
.word MDIOS_IRQHandler /* MDIOS */


 

Thanks & Regards,

K. Aravind