STM32F779AIY6 - What if NC pins are connected to GND?
Hello,
i just received some custom boards with a STM32F779AIY6 on it.
3V3 net and GND net have a short circuit when MCU is soldered, without MCU there is no short circuit.
I checked everything, it should be fine.
But what i just found was that the datasheet says:
NC ball must not be connected to GND nor to VDD.
But they are. They are all GND in my design. Big mistake.
Can this cause the short circtuit or should this be unrealistic and the problem must be somewhere else?
I hope someone can help me, it will be hard to remove those balls to test it.
Thanks a lot.