Skip to main content
hakan ozcan
Visitor II
December 11, 2017
Question

STM32F769I Eval Board Can Bus Example

  • December 11, 2017
  • 0 replies
  • 506 views
Posted on December 11, 2017 at 14:58

Hi everyone,

I am using STM32F769I Eval Board and i am trying to run the STM32Cube_FW_F7_V1.7.0 CAN_Networking example.

First i read the documentation and set the jumpers

+-------------+-----------------+

       |   Jumper    |       CAN1      |

       +-------------+-----------------+

       |   JP14      |      fitted     |

       |   JP19      |      1-2        |

       |   JP18      |      fitted     |

       +-------------+-----------------+

Then, i connected to device and try to set the bit rate 250 000 Kbit/s which is 1Mbit/s but i could not figure it out how.

And i am suspicious that this examples work properly, is there anyone having issues with that or anyone can set the bit rate to 250 000 Kbit/s?

By the way, i am new to this

Thans in advance,

#can-bus #can-bus-bit-timing #stm32f7-eval
This topic has been closed for replies.