Skip to main content
Associate
June 28, 2023
Solved

STM32F769i DISCO recovery to factory reset

  • June 28, 2023
  • 2 replies
  • 1713 views

I have purchased STM32F769 Discovery Kit. I'm new to this board usage. I tried an led blinking example using STM32CubeIDE. After Debugging the code I lost the factory default code and now nothing is showing on LCD display.

Is there a way to get back to the factory reset mode with LCD display and default settings? 

Kindly help me!

This topic has been closed for replies.
Best answer by Ozone

Not directly.
Once the Flash is erased, the code is gone.But the code you mention (usually called "demonstration project") is part of the resource downloads (software/firmware package), and you can directly flash it back onto the board.

I don't have a F769 discovery, but several other disco boards.

2 replies

Ozone
OzoneBest answer
Principal
June 28, 2023

Not directly.
Once the Flash is erased, the code is gone.But the code you mention (usually called "demonstration project") is part of the resource downloads (software/firmware package), and you can directly flash it back onto the board.

I don't have a F769 discovery, but several other disco boards.

Associate
June 29, 2023

Thanks a lot!