Skip to main content
TPier
Associate III
September 20, 2019
Solved

STM32F769 Discovery kit demo firmware

Hi,

I ran several test and example projects on the STM32F769 Discovery platform. I would like to reload the original demo firmware. According to the documentation, it should be available from the www.st.com/stm32f7-discovery webpage but I cannot find it again.

Could someone tell where I can find the original demo firmware for this kit ?

Many thanks in advance.

Best regards.

This topic has been closed for replies.
Piranha
PiranhaBest answer
Principal III
September 25, 2019

Compiled demo firmware can be found in STM32CubeF7 package:

\Projects\STM32F769I-Discovery\Demonstrations\STemWin\Binary\

11 replies

waclawek.jan
Super User
September 20, 2019

Good question. It's not among the compiled binaries (https://www.st.com/en/evaluation-tools/stm32-discovery-kits.html#resource click on Binary resources - no direct link courtesy of the idiotic "new look and feel" of the ST webpage).

ST, can you plese fix this?

JW

@Amel NASRI​  , @Imen DAHMEN​ 

ST Technical Moderator
September 25, 2019

Hello,

We raised your feedback internally to the appropriate team.

For the 32F769IDISCOVERY demo firmware, it will be published soon on the ST webpage.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
waclawek.jan
Super User
September 25, 2019

Hi @Imen DAHMEN​ ,

Thanks for the reply. I don't know if you have read the post below, too - there are more Disco demo binaries missing than just the 'F769Disco.

Jan

waclawek.jan
Super User
September 20, 2019

There are more firmwares missing, e.g. for the classic 'F4 DISCO (the 'F407 based one)

JW

waclawek.jan
Super User
September 20, 2019
TPier
TPierAuthor
Associate III
September 23, 2019

Many thanks.

For your info: the binaries do not load properly. As a consequence, for the full demo, the access to the "Embedded Wizard" demos crashes the system. For the Stm32Cube demo, some images are just garbage.

Verification of the upload gives the error "Data mismatch found at address 0x90000000 (byte = 0x00 instead of 0x99)". I did not get the time yet to investigate more ...

Best regards.

Piranha
PiranhaBest answer
Principal III
September 25, 2019

Compiled demo firmware can be found in STM32CubeF7 package:

\Projects\STM32F769I-Discovery\Demonstrations\STemWin\Binary\

TFlac
Associate III
September 25, 2019

Hello Community,

Yes, I went through this myself. The fact of the matter is there should not be BINARIES for example designs. There should be source files to allow the user to see what and how the design was done. If the source files were given then more people would learn the tool flows better. The key objective in this type of question to let ST know that we need more and better documentation.

I'm using the STM32F3 products and also the STM32_FW_F3 firmware package. The documentation for this firmware is no three years old. The CubeMX and CubeIDE are not mentioned as they did not exist yet. The example in the F3 firmware are great but they are hand written (no MX or CubeIDE). The only way I can get the MX to work is to cut and paste the source files from the example folder. There are no instructions on how to open these examples using CubeMX/IDE no where.

We as the ST community must let ST know we need latest documentation for the latest tools. I chose to use CubeIDE and MX. You will find it very difficult to have MX create the handwritten code designs that are in the firmware packages.

TPier
TPierAuthor
Associate III
September 26, 2019

Same report for the STM32F7 packages. All the examples are running out of the box (needing some tweaks with IAR Workbench). But it is really painful to create a new project from scratch with the STMCube tools.

However, examples are really nice and instructive. Thanks for this.