Skip to main content
Vaclav Zajic
Associate III
May 22, 2018
Question

stm32f767 usart2

  • May 22, 2018
  • 5 replies
  • 1550 views
Posted on May 22, 2018 at 15:07

Hello, 

I can not get usart2 working in asynchronous mode on STM32f767zi-nucleo.

My clock configuration function contains

PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USART2|RCC_PERIPHCLK_USART3|RCC_PERIPHCLK_CLK48;

PeriphClkInitStruct.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1;

In main() I call 

static void MX_USART2_UART_Init(void)

{

huart2.Instance = USART2;

huart2.Init.BaudRate = 115200;

huart2.Init.WordLength = /*UART_WORDLENGTH_7B*/UART_WORDLENGTH_8B;

huart2.Init.StopBits = UART_STOPBITS_1;

huart2.Init.Parity = UART_PARITY_NONE;

huart2.Init.Mode = UART_MODE_TX_RX;

huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;

huart2.Init.OverSampling = UART_OVERSAMPLING_16;

huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;

huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;

if (HAL_UART_Init(&huart2) != HAL_OK)

{

_Error_Handler(__FILE__, __LINE__);

}

}

When I try to send something to USART2 with HAL_UART_Transmit I get return code HAL_OK, but I can't  see anything on serial port.

Can you give me an advice?

Thank you

Vaclav 

    This topic has been closed for replies.

    5 replies

    waclawek.jan
    Super User
    May 22, 2018
    Posted on May 22, 2018 at 15:20

    Read back and check the relevant RCC, GPIO and UART registers.

    JW

    Vaclav Zajic
    Associate III
    May 22, 2018
    Posted on May 22, 2018 at 15:43

    After trying to send a message the USART2 registers look like this:

    CR1 0x0

    CR2 0x0

    CR3 0x0

    BRR 0x0

    GTPR 0x0

    RTOR 0x0

    RQR empty

    ISR 0xc0

    ICR empty

    RDR 0x0

    TDR 0x0

    Tesla DeLorean
    Guru
    May 22, 2018
    Posted on May 22, 2018 at 16:30

     ,

     ,

    Looks like the clock isn't actually enabled. USART2 on PA2/PA3 would look like this in a complete form. CubeMX spreads things all over the place. Check the pin/clock stuff generated in the MSP code

    void USART2_Init(void)

     ,

    {

     ,

     , GPIO_InitTypeDef , GPIO_InitStruct,

     , /* ♯ ♯ -1- Enable peripherals and GPIO Clocks ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ */

     ,

     , /* Enable GPIO TX/RX clock */

     ,

     , ,  ,__HAL_RCC_GPIOA_CLK_ENABLE(),

     ,

     , /* Enable USART2 clock */

     ,

     , ,  ,__HAL_RCC_USART2_CLK_ENABLE(),

     ,

     , ,  ,

     ,

     , /* ♯ ♯ -2- Configure peripheral GPIO ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ */

     ,

     , /* UART TX and RX GPIO pin configuration , */

     ,

     , GPIO_InitStruct.Pin , , , , , , = GPIO_PIN_2 | GPIO_PIN_3,

     ,

     , GPIO_InitStruct.Mode , , , , , = GPIO_MODE_AF_PP,

     ,

     , GPIO_InitStruct.Pull , , , , , = GPIO_PULLUP,

     ,

     , GPIO_InitStruct.Speed , , , , = GPIO_SPEED_FAST,

     ,

     , GPIO_InitStruct.Alternate = GPIO_AF7_USART2,

     , HAL_GPIO_Init(GPIOA, &,GPIO_InitStruct),

    /* ♯ ♯ -1- Configure the UART peripheral ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ */

     ,

     , /* Put the USART peripheral in the Asynchronous mode (UART Mode) */

     ,

     , /* UART configured as follows:

     ,

     , , , , , - Word Length = 8 Bits

     ,

     , , , , , - Stop Bit = One Stop bit

     ,

     , , , , , - Parity = None

     ,

     , , , , , - BaudRate = 9600 baud

     ,

     , , , , , - Hardware flow control disabled (RTS and CTS signals) */

     ,

     , UartHandle.Instance , , , , , , , = USART2,

     , UartHandle.Init.BaudRate , , = 115200,

     ,

     , UartHandle.Init.WordLength = UART_WORDLENGTH_8B,

     ,

     , UartHandle.Init.StopBits , , = UART_STOPBITS_1,

     ,

     , UartHandle.Init.Parity , , , , = UART_PARITY_NONE,

     ,

     , UartHandle.Init.HwFlowCtl , = UART_HWCONTROL_NONE,

     ,

     , UartHandle.Init.Mode , , , , , , = UART_MODE_TX_RX,

     ,

    ♯ ifdef UART_ADVFEATURE_NO_INIT

     ,

     , UartHandle.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT,

     ,

    ♯ endif

     , if (HAL_UART_DeInit(&,UartHandle) != HAL_OK)

     ,

     , {

     ,

     , , , Error_Handler(),

     ,

     , }

     , if (HAL_UART_Init(&,UartHandle) != HAL_OK)

     ,

     , {

     ,

     , , , Error_Handler(),

     ,

     , }

    }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Vaclav Zajic
    Associate III
    May 23, 2018
    Posted on May 23, 2018 at 09:11

    Hello, the problem was that I forgot to enable the USART clock by 

    __USART2_CLK_ENABLE. It works now. Thank you all.

    Vaclav