Skip to main content
dohzer
Associate II
Apr 5, 2017 10:42 AM UTC
Solved

STM32F767 SRAM1 Address

Posted on April 05, 2017 at 12:42

Looking at the STM32F767xx Datasheet (DocID029041 Rev 4), the SRAM1 address is listed as 0x20020000.

But the STM32F76xxx Reference Manual (DocID028270 Rev 2) lists this as 0x20010000 in several places:

  • Page 98/1896: 'BOOT_ADD0 = 0x8004: Boot from SRAM1 (0x2001 0000)'
  • Page 99/1896: 'BOOT_ADD1 = 0x8004: Boot from SRAM1 (0x2001 0000)'
  • Page 112

    /1896

    : 'BOOT_ADD1 = 0x8004: Boot from SRAM1 (0x2001 0000)'
  • Page 112/1896: 'BOOT_ADD0 = 0x8004: Boot from SRAM1 (0x2001 0000)'

Is this a typographical error?

#stm32f767 #stm32f767zi-nucleo #stm32f767zi-nucleo-board #stm32f7
This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Apr 5, 2017 1:26 PM UTC
Posted on April 05, 2017 at 15:26

Hi

Doherty.Rowan

,

I confirm the error you are reporting about the

SRAM1 address in the RM0410 and should be

0x2002 0000

.

I would inform you that the reference manual will be corrected in coming release.

Thank you for bringing this to our attention.

Best Regards

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

2 replies

ST Technical Moderator
Apr 5, 2017 12:29 PM UTC
Posted on April 05, 2017 at 14:29

Hi 

Thank you for your reported error. I will check this and come back to you as soon as possibe.

Thanks

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Imen.DBest answer
ST Technical Moderator
Apr 5, 2017 1:26 PM UTC
Posted on April 05, 2017 at 15:26

Hi

Doherty.Rowan

,

I confirm the error you are reporting about the

SRAM1 address in the RM0410 and should be

0x2002 0000

.

I would inform you that the reference manual will be corrected in coming release.

Thank you for bringing this to our attention.

Best Regards

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks