Question
STM32F746G Disco DAC_OUT1 & DAC_OUT2 access?
Posted on September 01, 2017 at 06:37
Hi,
I have an STM32F746G-DISCO board and I am running some DAC examples. I need physical access to PA4 (DAC_OUT1) and PA5 (DAC_OUT2) so I can display them both on the oscilloscope. The DAC example says you can access PA4 via Pin 17 on P1 (camera) connector. But that is tiny. Is there some other way I can access both DAC pins. How are people displaying both DAC channels on an oscilloscope for example if its hard to access these pins? Suggestions welcome :)
Cheers / Frank
#stm32f7-discovery #dac_out2 #dac_out1