Skip to main content
JChen.24
Associate III
September 28, 2021
Question

STM32f746G_DISCO board sdram configuration quesiton

  • September 28, 2021
  • 1 reply
  • 569 views

Hi,

In the STM32F746G_DISCO board, FMC_SDRAM example, how to decide these parameters? Which section does it specify from sdram MT48LC4M32B2B5 datasheet?

 SDRAM_Timing.LoadToActiveDelay   = 2;

 SDRAM_Timing.ExitSelfRefreshDelay = 6;

 SDRAM_Timing.SelfRefreshTime     = 4;

 SDRAM_Timing.RowCycleDelay       = 6;

 SDRAM_Timing.WriteRecoveryTime   = 2;

 SDRAM_Timing.RPDelay             = 2;

 SDRAM_Timing.RCDDelay            = 2;

 hsdram.Init.SDBank            = FMC_SDRAM_BANK1;

 hsdram.Init.ColumnBitsNumber  = FMC_SDRAM_COLUMN_BITS_NUM_8;

 hsdram.Init.RowBitsNumber     = FMC_SDRAM_ROW_BITS_NUM_12;

 hsdram.Init.MemoryDataWidth   = SDRAM_MEMORY_WIDTH;

 hsdram.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_4;

 hsdram.Init.CASLatency        = FMC_SDRAM_CAS_LATENCY_2;

 hsdram.Init.WriteProtection   = FMC_SDRAM_WRITE_PROTECTION_DISABLE;

 hsdram.Init.SDClockPeriod     = SDCLOCK_PERIOD;

 hsdram.Init.ReadBurst         = FMC_SDRAM_RBURST_ENABLE;

 hsdram.Init.ReadPipeDelay     = FMC_SDRAM_RPIPE_DELAY_0;

Thanks.

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
September 28, 2021

The timing parameters are in clock cycles for the FMC, need to convert into nanoseconds, and need to be within the specs in the datasheet

ie if it wants 35ns min, 30ns won't work, but 40ns would, if from a 100 MHz timing source (4 cycles).

CAS, RAS, rows, columns, banks, surely those are in the datasheet.

Memory width would depend on part and board. Couple of occasions ST has used 16-bit data bus, on 32-bit parts, due to cost/availability, and used half the SDRAM capacity.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..