Skip to main content
alexandertischner9
Visitor II
August 16, 2016
Question

STM32F746; USBH_Start/Stop issue

  • August 16, 2016
  • 1 reply
  • 686 views
Posted on August 16, 2016 at 13:29

Hello,

I want to read/write files on a usb stick in my application and I already have generated a project with the help of ST32CubeMX for my Nucleo-F746ZG board. The configuration in CubeMX is: -USB_OTG_FS, Host_Only -Mass Storage Host Class -FATFs: USB Disk My application follows this sequence: 1. read/write file on usb stick 2. disable usb operation. I do that, because otherwise the global usb_otg interrupt (OTG_FS_IRQHandler) would slow down step 3 (processing). 3. processing 4. enable usb operation 5. read/write file on usb stick Note: During all steps, the usb stick is connected to the STM32F7. Step 1 works, but after disabling and enabling the usb operation, the usb stick seems to be disconnected and I cannot read/write to the file in step 5. I tried to disalbe/enable the operation with USBH_Start and USBH_Stop. Here is my test application, that shall demonstrate the issue:

/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_TIM6_Init();
MX_SPI1_Init();
MX_TIM1_Init();
MX_I2C1_Init();
MX_I2C2_Init();
MX_FATFS_Init();
MX_USB_HOST_Init();
MX_CRC_Init(); 
//stop/start test 
volatile uint32_t cnt = 0;
while(1)
{
MX_USB_HOST_Process();
if (Appli_state == APPLICATION_READY)
{
MX_USB_HOST_Stop();
MX_USB_HOST_Start();
cnt++;
}
}

Note: MX_USB_HOST_Start/Stop are wrapper functions for USBH_Start/Stop. Appli_state is APPLICATION_READY only once. After Stop/Start was executed, Appli_state remains in APPLICATION_DISCONNECT. My thoughts: -I´m not sure if USBH_Start/Stop are the right API calls for my use case. -Maybe I should re-initialize the whole usb module + drivers Any ideas what is happening?
    This topic has been closed for replies.

    1 reply

    troy1818
    Associate III
    August 16, 2016
    Posted on August 16, 2016 at 14:29

    To call USBH_Stop just because you do not want any interrupts seems a bit harsh to me.

    Try and just disable the interrupt (NVIC) and enable it again. Or you can just set a flag when the interrupt is called, so when it is 0, it will just skip the function call inside the interrupt.