Skip to main content
Niklas Voi
Associate II
May 16, 2018
Question

STM32F746 + RTOS + LWIP Respond Time high / every second Paket dropped.

  • May 16, 2018
  • 0 replies
  • 376 views
Posted on May 16, 2018 at 16:13

Hi, i have big issues with a STM32F746 + RTOS + LWIP. Initialcode is generated by CubeMX.

The Problem: I ping with the device and every second paket get responded with a delay of 800-1000 ms or dropped/timeouted. There a 2 UDP-Services that accept pakets on two dedicated Ports,

they also have the same problem. If i increase the rate of UDP-Requests, the ICMP/UDP respond time is a very low ( a 1 ms ).

I think some periodic Task from the LWIP get not often enough called.

Had anyone an idea where to look ?

Best regards and Thanks,

Niklas
    This topic has been closed for replies.