STM32F730R8 __FPU_USED needed?
Hello all, I'd like to know if I'm making full use of the FPU on an F730 using SW4STM32/Eclipse. In project properties i set floating point hardware to fpV5-sp-d16 and the ABI to hardware. I also define __FPU_PRESENT & ARM_MATH_CM7 and set the library path and libraries. However, __FPU_PRESENT is automatically set to 0. If i change it to 1, the code works and doesn't seem to run any faster. Examining the assembly code (with fpu_present == 0 ) looks like proper fpu instructions and SCB_GetFPUType() returns 1, so maybe it doesn't matter? It's confusing.