Skip to main content
Brian Kennedy
Associate
Jan 11, 2018 5:31 PM UTC
Solved

STM32F723e-disco HS USB examples - Cube issues

Posted on January 11, 2018 at 18:31

I am currently trying to generate a new project for Keil as a HS Custom HID device (eventually it will be composite with another class) and have been encountering enumeration issues.  The code builds, loads, and runs, but my USB bus analyzer shows a steady streams of chirps, resets, and suspends instead of enumeration.  If I modify the project with the CubeMX tool to use FS instead, the project does appear to enumerate properly so is there something else simple I may be missing here? Are there any standalone HS USB reference examples for the STM32F723e-disco, because I haven't found any yet in the F7 Cube library?

#stm32f7-usb-device-hs
This topic has been closed for replies.
Brian Kennedy_2
Brian Kennedy_2Best answer
Visitor II
Jan 12, 2018 1:14 AM UTC
Posted on January 12, 2018 at 02:14

I sorted out my issues and it ended up being a bad cable (which still worked with FS).  That said, it still would be nice if there were some high speed USB examples.

2 replies

Brian Kennedy_2
Brian Kennedy_2Best answer
Visitor II
Jan 12, 2018 1:14 AM UTC
Posted on January 12, 2018 at 02:14

I sorted out my issues and it ended up being a bad cable (which still worked with FS).  That said, it still would be nice if there were some high speed USB examples.

Khouloud GARSI
ST Employee
Jan 16, 2018 3:07 PM UTC
Posted on January 16, 2018 at 15:07

Hello

Kennedy.Brian

,

There is an application titled 'HID_Standalone' found under the

http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-mcu-packages/stm32cubef7.html

firmware package:

STM32Cube_FW_F7_V1.8.0\Projects\STM32F723E-Discovery\Applications\USB_Device\HID_Standalone.

This application is a part of the USB Device Library package using STM32Cube firmware. It describes how to use the USB device application based on theHIDon the STM32F723xx devices.

To select the appropriate USB Core to work with, the macro define 'USE_USB_HS' is added within the compiler preprocessor (project : STM32F723E-DISCOVERY_USBD_HS).

To use the USB HS, you should connect the STM32F723E-Discovery board to the PC through the 'USB micro A-Male to A-Male' cable to the connector CN

Khouloud.