Question
STM32F722CV - USART1 RX Interrupt not working.
Hello, I am trying to communicate MCU with using USART1 but interrupt never triggered in MCU.
First I am using some definitions. Here is definitions for USART1.
#define USART1_PINS_PORT GPIOA
#define USART1_RX_PIN GPIO_PIN_10
#define USART1_TX_PIN GPIO_PIN_9
#define USART1_ALTERNATE_FUNC GPIO_AF7_USART1
#define USART1_GPIO_CLK_ENABLE() __HAL_RCC_GPIOA_CLK_ENABLE()
#define USART1_CLK_ENABLE() __HAL_RCC_USART1_CLK_ENABLE()
#define USART1_IRQ_NUM USART1_IRQn
UART_HandleTypeDef USART1_Handle; /* Put USART to asynchronous mode */My init function is :
void ml45_uart_init(void)
{
USART1_Handle.Instance = USART1;
USART1_Handle.Init.BaudRate = 115200;
USART1_Handle.Init.Mode = USART_MODE_TX_RX;
USART1_Handle.Init.WordLength = USART_WORDLENGTH_8B;
USART1_Handle.Init.StopBits = USART_STOPBITS_1;
USART1_Handle.Init.Parity = USART_PARITY_NONE;
USART1_Handle.Init.HwFlowCtl = UART_HWCONTROL_NONE;
USART1_Handle.Init.OverSampling = UART_OVERSAMPLING_16;
USART1_Handle.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
USART1_Handle.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if ( HAL_UART_DeInit(&USART1_Handle) != HAL_OK )
{
while ( 1 )
{
/* UART INITIALIZATION FAILED */
}
}
if ( HAL_UART_Init(&USART1_Handle) != HAL_OK )
{
while ( 1 )
{
/* UART INITIALIZATION FAILED */
}
}
}And here is my msp init and msp deinit function :
void HAL_UART_MspInit(UART_HandleTypeDef *husart)
{
/* Enable Peripherals */
USART1_CLK_ENABLE();
USART1_GPIO_CLK_ENABLE();
GPIO_InitTypeDef GPIO_InitStructure;
/* Init RX TX Pin */
GPIO_InitStructure.Pin = USART1_TX_PIN | USART1_RX_PIN;
GPIO_InitStructure.Mode = GPIO_MODE_AF_PP;
GPIO_InitStructure.Pull = GPIO_NOPULL;
GPIO_InitStructure.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStructure.Alternate = USART1_ALTERNATE_FUNC;
HAL_GPIO_Init(USART1_PINS_PORT, &GPIO_InitStructure);
/* Arrange interrupt priority then enable it for USART1 */
__HAL_USART_ENABLE_IT(husart, USART_IT_RXNE);
__HAL_USART_CLEAR_IT(husart, USART_IT_TXE);
HAL_NVIC_SetPriority(USART1_IRQ_NUM, 0, 1);
HAL_NVIC_EnableIRQ(USART1_IRQ_NUM);
}
/**
* @brief UART MSP De-Initialization
* This function frees the hardware resources used in this example:
* - Disable the Peripheral's clock
* - Revert GPIO and NVIC configuration to their default state
* @param huart: UART handle pointer
* @retval None
*/
void HAL_UART_MspDeInit(UART_HandleTypeDef *husart)
{
(void)husart;
__HAL_RCC_USART1_FORCE_RESET();
__HAL_RCC_USART1_RELEASE_RESET();
HAL_GPIO_DeInit(USART1_PINS_PORT, USART1_RX_PIN);
HAL_GPIO_DeInit(USART1_PINS_PORT, USART1_TX_PIN);
HAL_NVIC_DisableIRQ(USART1_IRQ_NUM);
}And lastly here is my interrupt routine :
void USART1_IRQHandler(void)
{
volatile uint32_t ISR_shadow = USART1_Handle.Instance->ISR;
}I put debug point in USART1_IRQHandler. Program can not reach at this point.
I am sure with the sending side of USART. This part is working.
So What is mcu's problem ? Is mine initialization code is wrong ?
Thanks for answers.