Skip to main content
Associate
Jan 13, 2025 5:43 PM UTC
Solved

STM32F7 RS485 DE Enable Not working

Hi 

I have been trying to configure the RS485 and trying to enable DE line. Though I have configured the DE line correctly, but still when HAL_UART_Transmit() is called, it just stays low and never get enabled for D to tranmit the data to the destination. Here is the code:

 

 

void UART6_Init(void) {

 

 

__HAL_RCC_USART6_CLK_ENABLE();

__HAL_RCC_GPIOG_CLK_ENABLE();

__HAL_RCC_GPIOB_CLK_ENABLE();

 

GPIO_InitTypeDef GPIO_InitStruct;

 

// UART TX (PG14) and RX (PG9) pin configuration

GPIO_InitStruct.Pin = GPIO_PIN_14 | GPIO_PIN_9;

GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;

GPIO_InitStruct.Alternate = GPIO_AF8_USART6;

HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);

 

// DE (PB0) pin configuration for alternate function

GPIO_InitStruct.Pin = GPIO_PIN_0;

GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; // Alternate function for DE

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;

GPIO_InitStruct.Alternate = GPIO_AF8_USART6;

HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 

 

// UART initialization

huart6.Instance = USART6;

huart6.Init.BaudRate = 9600;

huart6.Init.WordLength = UART_WORDLENGTH_8B;

huart6.Init.StopBits = UART_STOPBITS_1;

huart6.Init.Parity = UART_PARITY_NONE;

huart6.Init.Mode = UART_MODE_TX_RX;

huart6.Init.HwFlowCtl = UART_HWCONTROL_NONE;

huart6.Init.OverSampling = UART_OVERSAMPLING_16;

 

// Enable RS-485 DE mode with 1-bit assertion and de-assertion time

if (HAL_RS485Ex_Init(&huart6, UART_DE_POLARITY_HIGH, 2, 2) != HAL_OK) {

printf("Failed to enable RS-485 DE mode!\n\r");

while (1); // Stay here on error

}

 

printf("USART_CR3:==> 0x%08lx\r\n", USART6->CR3); // Should have DEM bit set

printf("USART_CR1==>: 0x%08lx\r\n", USART6->CR1); // Should have DEAT and DEDT bits set

 

 

// Enable USART6 interrupt with priority 1

HAL_NVIC_SetPriority(USART6_IRQn, 1, 0);

HAL_NVIC_EnableIRQ(USART6_IRQn);

 

//output for the above printf:

//USART_CR3:==> 0x00004000
//USART_CR1==>: 0x0084000d

}

 

void MinimalTest(void) {

uint8_t testMsg[] = "RS-485 Test\n";

 

while (1) {

HAL_UART_Transmit(&huart6, testMsg, sizeof(testMsg) - 1, HAL_MAX_DELAY);

HAL_Delay(10000);

 

 

}

}

 

 

int main(void)

{

/* Configure the MPU attributes */

MPU_Config();

 

/* Enable the CPU Cache */

CPU_CACHE_Enable();

 

HAL_Init();

 

/* Configure the system clock to 216 MHz */

SystemClock_Config();

 

 

UART6_Init();

MinimalTest();

 

}

 

 DE line never gets enabled.

I have tried using the GPIO way of toggling the PB0, as that works perfectly fine,

so it is confirmed that there can be any issue with connections or the hardware settings.

I just wanted to remove GPIO manual toggling and wanted to use DE Enable line to go to high

when USART is trying to send the data on the RS485.

The board i am using is:

Nucleo-144 (STM32f767ZI)

Any comments what can be the issue, will be really helpful.

 

This topic has been closed for replies.
KnarfB
KnarfBBest answer
Super User
Jan 13, 2025 6:28 PM UTC

DS11532 Rev 8 Table 13. STM32F765xx, STM32F767xx, STM32F768Ax, and STM32F769xx alternate
function mapping says UART4_CTS for PB0 AF8, not USART6.

 

5 replies

KnarfB
Super User
Jan 13, 2025 6:20 PM UTC

The STM32CubeMX generated code for my STM32L432KC looks the same and works here.

hth

KnarfB

KnarfB
KnarfBBest answer
Super User
Jan 13, 2025 6:28 PM UTC

DS11532 Rev 8 Table 13. STM32F765xx, STM32F767xx, STM32F768Ax, and STM32F769xx alternate
function mapping says UART4_CTS for PB0 AF8, not USART6.

 

DESTM32Author
Associate
Jan 13, 2025 6:39 PM UTC

This is from STM32f7xx:

 

/**

* @brief AF 8 selection

*/

#define GPIO_AF8_UART4 ((uint8_t)0x08U) /* UART4 Alternate Function mapping */

#define GPIO_AF8_UART5 ((uint8_t)0x08U) /* UART5 Alternate Function mapping */

#define GPIO_AF8_USART6 ((uint8_t)0x08U) /* USART6 Alternate Function mapping */

#define GPIO_AF8_UART7 ((uint8_t)0x08U) /* UART7 Alternate Function mapping */

#define GPIO_AF8_UART8 ((uint8_t)0x08U) /* UART8 Alternate Function mapping */

#define GPIO_AF8_SPDIFRX ((uint8_t)0x08U) /* SPIDIF-RX Alternate Function mapping */

#define GPIO_AF8_SAI2 ((uint8_t)0x08U) /* SAI2 Alternate Function mapping */

#if defined (STM32F765xx) || defined(STM32F767xx) || defined(STM32F769xx) || defined(STM32F777xx) || defined(STM32F779xx)

#define GPIO_AF8_SPI6 ((uint8_t)0x08U) /* SPI6 Alternate Function mapping */

#endif /* STM32F767xx || STM32F769xx || STM32F777xx || STM32F779xx */

 

And i am using USART6

DESTM32Author
Associate
Jan 13, 2025 6:26 PM UTC

Now that is interesting, I checked the datasheet of STM32L432KC , it specifically mentions in:

Section 3.24:
These interfaces provide asynchronous communication, IrDA SIR ENDEC support,
multiprocessor communication mode, single-wire half-duplex communication mode and
have LIN Master/Slave capability. They provide hardware management of the CTS and RTS
signals, and RS485 Driver Enable. They are able to communicate at speeds of up to
10Mbit/s.

But in the datasheet for STM32F767ZI, nothing of that sort has been mentioned, apart in the Table in it. Now, I doubt whether STM32F7 really support DE Line automatically or not.