Skip to main content
Christensen.Tyler
Associate II
October 31, 2018
Question

STM32F7 QSPI AR-Register False Update

  • October 31, 2018
  • 0 replies
  • 479 views

This has been discussed in two other threads, one brought up by someone else and another by myself when I thought I found a solution but it ended up being a fake solution.

https://community.st.com/s/question/0D50X00009XkgwcSAB/stm32f7-quadspi-and-the-data-cache-odd-behaviour

https://community.st.com/s/question/0D70X0000068Xn8/do-interrupt-priorities-have-to-start-at-zero

I can now reproduce this on a discover board with no private IP in the project, so I'll post the project publicly. It is a heavily stripped down project that has the USB driver, our company's public communications API, and a few random functions here and there that shouldn't matter but somehow do. At this point, if I remove just about anything else, even functions that never get called or interrupt handlers for interrupts that aren't even enabled, the problem goes away. Changing to anything below -O3 also makes the problem go away, but I need root cause before I can move on from this bug.

Here is the Keil uVision project: https://www.dropbox.com/s/1mv29boljscgnms/QSPI_Bug.zip?dl=0

This can be run directly on an STM32F746G-DISCO board. You do have to remove R64 jumper and move it to R63 to activate VBUS sense on the USB FS line.

To reproduce the problem:

  1. Move R64 to R63 on the discover board.
  2. Load the program with the Keil debugger running. Monitor the QUADSPI->AR register in a watch window or the peripheral viewer. Notice that it is not 0 (it's changed at the beginning of main()).
  3. Connect a USB micro cable to your computer to the USB FS port.
  4. Wait two seconds, and then unplug that cable.
  5. Plug the cable back in.
  6. Observe that QUADSPI->AR just changed to 0.

What changed it? I just cannot figure it out. If you set a memory write watch on the QUADSPI->AR register (0xA0001018) it never trips despite watching the register change.

I'll open a support ticket with ST to get this looked at, but figured I'd make the post public so that everyone can see the results and maybe a community member will be able to contribute to figuring this one out!

    This topic has been closed for replies.