Skip to main content
imtiaz
Associate III
Dec 6, 2016 1:50 AM UTC
Solved

STM32F7 EVAL Boot mode

Posted on December 06, 2016 at 02:50

Hi,

I am trying to put the STM32F769i_EVAL into system BOOT mode. I can do this successfully with an F429 Eval but not with the F7 Eval. I can see that when I reset it the normal program does not run , indicating that Bot mode has been entered , but it does not respond to the 0x7f (connect ) command.

I've tried with both my own known working software loader and the ST flash loader. I am using UART 1 which is otherwise working. Ive tries various baudrates down to 9600.

I am pulling up the Boot pin JP1 directly to VDD and resetting the board.

Many Thanks

Imtiaz

#stm32f7-boot-mode
This topic has been closed for replies.
Nesrine M_O
Nesrine M_OBest answer
Associate
Dec 23, 2016 3:10 PM UTC
Posted on December 23, 2016 at 16:10

Hi

abdullah.abdullah

‌,

  • I recommend you to remove the R124 from your evaluation board then try the test.
  • keep us informed about the result

-Nesrine-

Ifmy suggestanswers your question, please mark it as correct.

16 replies

imtiaz
imtiazAuthor
Associate III
Jan 9, 2017 7:57 PM UTC
Posted on January 09, 2017 at 20:57

PA5 is the SPI1 bootloader SCK - AN2606 page 175.

SPI1_SCK pin Input PA5 pin: Slave clock line, used in Push-pull pull-down mode