Skip to main content
Grozea.Ion
Associate III
June 30, 2017
Question

Stm32f7 Discovery - UART DMA help needed

Posted on June 30, 2017 at 10:47

Hi,

I have the following issue when using the attached code:

board->computer

ABCDE\r\n

the computer dosent receive anything

i send from the computer '11

\r\n

'

the board reply is ABCD

basically there is one step delay between receiving/sending the message

the code in the main  is shown below

int main(void)

{

MPU_Config();

CPU_CACHE_Enable();

&sharpifdef RTE_CMSIS_RTOS // when using CMSIS RTOS

osKernelInitialize(); // initialize CMSIS-RTOS

&sharpendif

HAL_Init();

BSP_SDRAM_Init();

/* Configure the System clock to have a frequency of 216 MHz */

SystemClock_Config();

myGPIO_Init();

myNVIC_Init();

myADC_Init();

myUART_Init();

...

//&sharpifdef RTE_CMSIS_RTOS // when using CMSIS RTOS

Init_GUIThread();

osKernelStart(); // start thread execution

//&sharpendif

// startFIFO();

myTime = HAL_GetTick();

for(cnt=0; cnt<7;cnt++)

TxBuffer[cnt] = cnt+65;

TxBuffer[7] = '\n';

SendToXbee(8);

while (1)

{

Battery_Val = getBattery();

if(HAL_GetTick() > myTime)

{

myToogle = !myToogle;

if(myToogle){

//XBeeOn;

myRxSize = Xbee_available();

if(myRxSize){

printf('Buffer has %d bytes\r\n', myRxSize);

for(cnt = 0; cnt < myRxSize; cnt++)

TxBuffer[cnt] = Xbee_get();

TxBuffer[cnt++] = '\r';

TxBuffer[cnt++] = '\n';

SendToXbee(myRxSize+2);

}

//printf('DMA data remaining: %d \r\n', myDMA_Remain);

//sprintf((char *)TxBuffer, 'Battery Value is %d \r\n', Battery_Val);

//SendToXbee(TxBuffer, sizeof(TxBuffer));

}else {

//XBeeOff;

}

myTime += 50;

}

osDelay(10);

}

Can anyone help me to understand what i am doing wrong?

Thank you

#dma #uart #ring-buffer #stm32f7-discovery
This topic has been closed for replies.