Skip to main content
Vitalii Mitko
Visitor II
May 26, 2017
Question

STM32F7 Disco USB3320

  • May 26, 2017
  • 0 replies
  • 458 views
Posted on May 26, 2017 at 18:49

STM32F7 Disco. I'm using the cube and keil.

So I got to HS, start with simple VCP, on FS USB it is correctly defined (after I removed VBUS sensing).

I generate the same empty project only for 2.0, on board the USB3320, the pins all match (in the cube I used not the choice of the chip but the choice of the board), VBUS tried both versions, the PC does not see the device.

Who raised this interface can tell you where to include or how to generate the code correctly?

P.s. The jumpers on the feeder are correct.

#stm32f7-usb-usb3320
This topic has been closed for replies.