STM32F7 DISCO : Demo not finding any audio/video files ?
Was anyone succesful in playing audio or video files with the demo sw ? My demo sw could not find any file on USB or SDcard.
I tried both USB-Ports ( but not the USB-Debugger port ) with different adapter cables included one from an other ST Eva-Kit. The files on SDcard and USB Memory stick are the same. Most of the files are from the other ST-Eva-Kit. I added more files of every type (mp3, wav, flv, mp4, emf) I can think of.
In file select menu you can select between two ''drives'' ( ''0'' and ''1''). What is drive ''0'' and what is drive ''1'' ? USB HS and FS or USB (HS/FS?) and SDcard or ???
Or do I need a special directory tree on the drives ?
Or a special file system (FAT16/32 or ???)
Thanks for your help.