Skip to main content
manuel2399
Associate
November 25, 2015
Question

STM32F7 Debugging in Eclipse

  • November 25, 2015
  • 1 reply
  • 657 views
Posted on November 25, 2015 at 15:51

Hello,

I need some help with the installation of a STM32F7 Discovery Board.

I would like to debug it via the integrated ST-Link/V2-1 in Eclipse

So far I use the Atollic GDB and OpenOCD (with the STM32F7 support: 

http://gnutoolchains.com/arm-eabi/openocd/

 )

But when I start OpenOCD I receive following errors:

Open On-Chip Debugger 0.9.0 (2015-08-15-12:41)

Licensed under GNU GPL v2

For bug reports, read

http://openocd.org/doc/doxygen/bugs.html

Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD

adapter speed: 2000 kHz

adapter_nsrst_delay: 100

srst_only separate srst_nogate srst_open_drain connect_deassert_srst

Info : Unable to match requested speed 2000 kHz, using 1800 kHz

Info : Unable to match requested speed 2000 kHz, using 1800 kHz

Info : clock speed 1800 kHz

Info : STLINK v2 JTAG v24 API v2 SWIM v11 VID 0x0483 PID 0x374B

Info : using stlink api v2

Info : Target voltage: 3.228947

Info : STM32F746.cpu: hardware has 0 breakpoints, 0 watchpoints

Error: jtag status contains invalid mode value - communication failure

Polling target STM32F746.cpu failed, trying to reexamine

Examination failed, GDB will be halted. Polling again in 100ms

Info : Previous state query failed, trying to reconnect

Error: jtag status contains invalid mode value - communication failure

Polling target STM32F746.cpu failed, trying to reexamine

Examination failed, GDB will be halted. Polling again in 300ms

It seems like there is no JTAG communication. But where can I change it to SWD?

Did anyone managed to debug a STM32F7 with Eclipse?
    This topic has been closed for replies.

    1 reply

    MUHAMMET YÜCEL
    Visitor II
    May 22, 2017
    Posted on May 22, 2017 at 10:13

    Hi,

    i have a similar issue. My stm32f746-disco board is not communicating anymore.

    nor st-link utility or firmware update program cannot see st-link.

    please help.