Skip to main content
Associate II
April 18, 2024
Solved

STM32F7 crash on HAL_UART_Transmit

Hello,

 

My STM32F7 crash after Reinit the UART :

 

- I have an UART for my RS232, and I can communicate to 2 devices by this RS232. So the customers choose on which device he want to send data, then I configure internals variables and the UART baudrate and flow control.

 

- So I use the next fonction to reinit my UART :

 

void RS232_Link_USART1_UART_ReInit(uint32_t BaudRate, uint32_t FlowCtrl)
{
 HAL_UART_Abort_IT(&huart1);

 HAL_UART_DeInit(&huart1);

 huart1.Init.BaudRate = BaudRate;
 huart1.Init.HwFlowCtl = FlowCtrl;

 if (HAL_UART_Init(&huart1) != HAL_OK)
 {
 Error_Handler();
 }

 uint8_t buff;
 if (HAL_UART_Receive_IT(&huart1, &buff, 1) != HAL_OK) {
 Error_Handler();
 }
}

 

 

 - This code works for 1 device but not for the other device. The thing that change is that the device which occure the crash send datas back after a transmit but we don't treat them. If I comment the part "HAL_UART_Receive_IT" it works, but I want to resolve the problem because it can maybe happen with the other device.

 

- Then the STM32 crash in the function :

 

HAL_StatusTypeDef HAL_UART_Transmit(UART_HandleTypeDef *huart, const uint8_t *pData, uint16_t Size, uint32_t Timeout)
{
 const uint8_t *pdata8bits;
 const uint16_t *pdata16bits;
 uint32_t tickstart;

 /* Check that a Tx process is not already ongoing */
 if (huart->gState == HAL_UART_STATE_READY)
 {
 if ((pData == NULL) || (Size == 0U))
 {
 return HAL_ERROR;
 }

 __HAL_LOCK(huart);

 huart->ErrorCode = HAL_UART_ERROR_NONE;
 huart->gState = HAL_UART_STATE_BUSY_TX;

 /* Init tickstart for timeout management */
 tickstart = HAL_GetTick();

 huart->TxXferSize = Size;
 huart->TxXferCount = Size;

 /* In case of 9bits/No Parity transfer, pData needs to be handled as a uint16_t pointer */
 if ((huart->Init.WordLength == UART_WORDLENGTH_9B) && (huart->Init.Parity == UART_PARITY_NONE))
 {
 pdata8bits = NULL;
 pdata16bits = (const uint16_t *) pData;
 }
 else
 {
 pdata8bits = pData;
 pdata16bits = NULL;
 }

 __HAL_UNLOCK(huart);

 while (huart->TxXferCount > 0U)
 {
 if (UART_WaitOnFlagUntilTimeout(huart, UART_FLAG_TXE, RESET, tickstart, Timeout) != HAL_OK)
 {
 return HAL_TIMEOUT;
 }
 if (pdata8bits == NULL)
 {
 huart->Instance->TDR = (uint16_t)(*pdata16bits & 0x01FFU);
 pdata16bits++;
 }
 else
 {
 huart->Instance->TDR = (uint8_t)(*pdata8bits & 0xFFU);
 pdata8bits++;
 }
 huart->TxXferCount--;
 }

 if (UART_WaitOnFlagUntilTimeout(huart, UART_FLAG_TC, RESET, tickstart, Timeout) != HAL_OK)
 {
 return HAL_TIMEOUT;
 }

 /* At end of Tx process, restore huart->gState to Ready */
 huart->gState = HAL_UART_STATE_READY;

 return HAL_OK;
 }
 else
 {
 return HAL_BUSY;
 }
}

 

 at this instruction :

 

huart->Instance->TDR = (uint8_t)(*pdata8bits & 0xFFU);

 

 

 I dertermined that the problem is the variable "pdata8bits" but I don't know what's happening...

 

Thanks

This topic has been closed for replies.
PierreG-SBest answer
Associate II
April 18, 2024

Ok I found, just a buffer error about the :

uint8_t buff;
if (HAL_UART_Receive_IT(&huart1, &buff, 1) != HAL_OK)

 

1 reply

PierreG-SAuthorBest answer
Associate II
April 18, 2024

Ok I found, just a buffer error about the :

uint8_t buff;
if (HAL_UART_Receive_IT(&huart1, &buff, 1) != HAL_OK)