Skip to main content
dheerajdake9
Associate III
Apr 13, 2021 11:54 AM UTC
Solved

STM32F7 Configurable Interrupt Priority levels

Hello ST,

From datasheet(PM0253),

The SHPR1-SHPR3 registers set the priority level, 0 to 255 of the exception handlers that have configurable priority.

Also from datasheet,

Each PRI_n field is 8 bits wide, but the processor implements only bits[7:M] of each field, and bits[M-1:0] read as zero and ignore writes.

What is the value of M? How does this relate to Binary point priority grouping?

Thanks

Dheeraj

This topic has been closed for replies.
dheerajdake9
dheerajdake9Best answer
Associate III
Apr 14, 2021 8:54 AM UTC

I got the answer for this. The value of M depends on the value of priGroup set in AIRCR register. The range is described in Priority Grouping table 56. For example, if PRIGROUP is 0b001, M is 2.

1 reply

dheerajdake9
dheerajdake9AuthorBest answer
Associate III
Apr 14, 2021 8:54 AM UTC

I got the answer for this. The value of M depends on the value of priGroup set in AIRCR register. The range is described in Priority Grouping table 56. For example, if PRIGROUP is 0b001, M is 2.